PartObject Class¶
-
class
NXOpen.Preferences.
PartObject
¶ Bases:
object
Represents the set of object preferences applicable to entire part.
All the preferences available at UG GUI for object can be set by using this class except work layer. Work Layer should be set by using
NXOpen.Layer.LayerManager
class which holds a work layer property. To obtain an instance of this class, refer toNXOpen.Preferences.PartPreferences
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
FaceAnalysis | Returns or sets the face analysis flag for Solid and Sheets |
PartiallyShaded | Returns or sets the partially shaded flag for Solid and Sheets |
Translucency | Returns or sets the translucency value |
Methods¶
Method | Description |
---|---|
ConvertColorNumberToRGBValue | Converts color number to RGB constituents. |
ConvertRGBValueToColorNumber | Converts RGB color constituents to color number. |
GetColor | Returns the current color value for specified type. |
GetLegacyLineWidthMap | Gets line width map that is used to convert legacy line widths to new line widths. |
GetLineFont | Returns the current line font for specified object type @return |
GetWidth | Returns the current width for specified object type @return |
MigrateLegacyLineWidths | Migrates line width attributes stored in the part file to corresponding new line widths. |
SetColor | Sets the color. |
SetLegacyLineWidthMap | Sets line width map that is used to convert legacy line widths to new line widths. |
SetLineFont | Sets line font for specified object type |
SetWidth | Sets width for specified object type |
Enumerations¶
PartObjectColorSelection Enumeration | Describes whether color of object is not changed or it is default color or it is defined by user |
PartObjectLineFontType Enumeration | Represents the available types for font |
PartObjectObjectType Enumeration | Describes all available Types for object selection |
PartObjectWidthType Enumeration | Describes the available types for width |
Property Detail¶
FaceAnalysis¶
-
PartObject.
FaceAnalysis
¶ Returns or sets the face analysis flag for Solid and Sheets
-------------------------------------
Getter Method
Signature
FaceAnalysis()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceAnalysis(faceAnalysis)
Parameters: faceAnalysis (bool) – New in version NX3.0.0.
License requirements: None.
PartiallyShaded¶
-
PartObject.
PartiallyShaded
¶ Returns or sets the partially shaded flag for Solid and Sheets
-------------------------------------
Getter Method
Signature
PartiallyShaded()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartiallyShaded(partiallyShaded)
Parameters: partiallyShaded (bool) – New in version NX3.0.0.
License requirements: None.
Translucency¶
-
PartObject.
Translucency
¶ Returns or sets the translucency value
-------------------------------------
Getter Method
Signature
Translucency()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Translucency(translucency)
Parameters: translucency (int) – New in version NX3.0.0.
License requirements: None.
Method Detail¶
ConvertColorNumberToRGBValue¶
-
PartObject.
ConvertColorNumberToRGBValue
¶ Converts color number to RGB constituents.
The color number passed should be between 1 to 216
Signature
ConvertColorNumberToRGBValue(colorNumber)
Parameters: colorNumber (int) – Color value Returns: Equivalent RGB constituents Return type: NXOpen.Preferences.ViewVisualizationSpecialEffectsColorRGB_Struct
New in version NX3.0.0.
License requirements: None.
ConvertRGBValueToColorNumber¶
-
PartObject.
ConvertRGBValueToColorNumber
¶ Converts RGB color constituents to color number.
The Red, Green and Blue color constituents should be between 0 to 255.
Signature
ConvertRGBValueToColorNumber(fogColorRgbValue)
Parameters: fogColorRgbValue ( NXOpen.Preferences.ViewVisualizationSpecialEffectsColorRGB_Struct
) –Returns: Equivalent color value Return type: int New in version NX3.0.0.
License requirements: None.
GetColor¶
-
PartObject.
GetColor
¶ Returns the current color value for specified type.
The equivalent RGB values can be found by calling
ConvertColorNumberToRGBValue()
Red Component is ((((216 - color_number) % 36)/6)* 51) Green component is (((216 - color_number)/36) * 51) Blue is (((216 - color_number) % 6)* 51). So for example if returned color value is 47 then Red is ((((216 - 47) % 36)/6)* 51) = (((169 % 36)/6)* 51) = ((25/6)* 51) = 4*51 = 204 Green is (((216 - 47)/36) * 51) = ((169/36) * 51) = 4*51 = 204 Blue is (((216 - 47) % 6)* 51) = ((169 % 6)* 51) = 1*51 = 51
Signature
GetColor(type)
Parameters: type ( NXOpen.Preferences.PartObjectObjectType
) –Returns: Return type: int New in version NX3.0.0.
License requirements: None.
GetLegacyLineWidthMap¶
-
PartObject.
GetLegacyLineWidthMap
¶ Gets line width map that is used to convert legacy line widths to new line widths.
Following widths are considered as legacy line widths.
Preferences.PartObjectWidthType.ThinWidth
Preferences.PartObjectWidthType.NormalWidth
Preferences.PartObjectWidthType.ThickWidth
New line widths contain corresponding line widths for above three legacy line widths respectively. New line widths start at
Preferences.PartObjectWidthType.WidthOne
.Signature
GetLegacyLineWidthMap()
Returns: Array of 3 new widths each corresponding to a legacy width. First element corresponds to Thin width Second element corresponds to Normal width Third element corresponds to Thick width. :rtype: list of
NXOpen.Preferences.PartObjectWidthType
New in version NX10.0.0.
License requirements: None.
GetLineFont¶
-
PartObject.
GetLineFont
¶ Returns the current line font for specified object type
Signature
GetLineFont(type)
Parameters: type ( NXOpen.Preferences.PartObjectObjectType
) –Returns: Return type: NXOpen.Preferences.PartObjectLineFontType
New in version NX3.0.0.
License requirements: None.
GetWidth¶
-
PartObject.
GetWidth
¶ Returns the current width for specified object type
Signature
GetWidth(type)
Parameters: type ( NXOpen.Preferences.PartObjectObjectType
) –Returns: Return type: NXOpen.Preferences.PartObjectWidthType
New in version NX3.0.0.
License requirements: None.
MigrateLegacyLineWidths¶
-
PartObject.
MigrateLegacyLineWidths
¶ Migrates line width attributes stored in the part file to corresponding new line widths.
The migration is performed based on the legacy line width map stored in the part file.
See
Preferences.PartObject.GetLegacyLineWidthMap()
Line widths of various displayable objects such as solids, wireframe, drawing views etc. will be updated to new line widths. Display is regenerated if necessary to reflect the changes. A displayable object, that already has new line width assigned to it, is not affected.
Signature
MigrateLegacyLineWidths()
Returns: At least one legacy line width attribute has been migrated. :rtype: bool
New in version NX10.0.0.
License requirements: None.
SetColor¶
-
PartObject.
SetColor
¶ Sets the color.
For Default color pass -2 as color value and for no change pass -1. For other color calculate the color in RGB format. If you pass R value of Red component G value of Green and B value of Blue the color will be: color = (((255-R)/51)*6 + ((255-G)/51)*36 + ((255-B)/51)*1) + 1 ; Where R G and B values are between 0 and 255 . So for Green (0,255,0)we will pass color = (((255-0)/51)*6 + ((255-255)/51)*36 + ((255-0)/51)*1) + 1 = 30+0+5+1 = 36 The equivalent color number value can be found by calling
ConvertRGBValueToColorNumber()
Signature
SetColor(type, color)
Parameters: - type (
NXOpen.Preferences.PartObjectObjectType
) – - color (int) – Specified Color
New in version NX3.0.0.
License requirements: None.
- type (
SetLegacyLineWidthMap¶
-
PartObject.
SetLegacyLineWidthMap
¶ Sets line width map that is used to convert legacy line widths to new line widths.
See
Preferences.PartObject.GetLegacyLineWidthMap()
The new line widths used to map legacy line width are in logical order; i.e.;
Preferences.PartObjectWidthType.ThinWidth
maps to a smaller width value compared toPreferences.PartObjectWidthType.NormalWidth
and so on. Otherwise, the legacy line width map will be rejected.Signature
SetLegacyLineWidthMap(newLineWidths)
Parameters: newLineWidths (list of NXOpen.Preferences.PartObjectWidthType
) – Array of 3 new widths each corresponding to a legacy width. First element corresponds to Thin width Second element corresponds to Normal width Third element corresponds to Thick width.New in version NX10.0.0.
License requirements: None.
SetLineFont¶
-
PartObject.
SetLineFont
¶ Sets line font for specified object type
Signature
SetLineFont(type, lineFont)
Parameters: - type (
NXOpen.Preferences.PartObjectObjectType
) – - lineFont (
NXOpen.Preferences.PartObjectLineFontType
) –
New in version NX3.0.0.
License requirements: None.
- type (
SetWidth¶
-
PartObject.
SetWidth
¶ Sets width for specified object type
Signature
SetWidth(type, width)
Parameters: - type (
NXOpen.Preferences.PartObjectObjectType
) – - width (
NXOpen.Preferences.PartObjectWidthType
) –
New in version NX3.0.0.
License requirements: None.
- type (