PartObjectColorSelection Enumeration

NXOpen.Preferences.PartObject.ColorSelection is an alias for NXOpen.Preferences.PartObjectColorSelection

class NXOpen.Preferences.PartObjectColorSelection

Bases: object

Describes whether color of object is not changed or it is default color or it is defined by user

Enum Members

Enum Member Enum Member Description
NoChange
No Change
DefaultColor
Default Color
Color
User Defined Color
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.