PartObjectLineFontType Enumeration

NXOpen.Preferences.PartObject.LineFontType is an alias for NXOpen.Preferences.PartObjectLineFontType

class NXOpen.Preferences.PartObjectLineFontType

Bases: object

Represents the available types for font

Enum Members

Enum Member Enum Member Description
PartDefault
Default Value from Part
Solid
Solid
Dashed
Dashed
Phantom
Phantom
Centerline
Centerline
Dotted
Dotted
LongDashed
Long Dashed
DottedDashed
Dotted Dashed
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.