ReflectionDataBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
ReflectionDataBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.ReflectionData
builderTo create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateReflectionDataBuilder()
Default values.
Property Value IsReflectData 1 IsReflectTraceCurve 0 IsRefractData 0 IsRefractTraceCurve 0 ReflectAccuracy 20 RefractionIndex 1.5 Resolution Medium Thickness 5 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
EyePoint | Returns or sets the eye point |
IsReflectData | Returns or sets whether to create reflection data as output or not |
IsReflectTraceCurve | Returns or sets whether to create reflection trace curves as output or not |
IsRefractData | Returns or sets whether to create refraction data as output or not |
IsRefractTraceCurve | Returns or sets whether to create refraction trace curves as output or not |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReflectAccuracy | Returns or sets the customized reflection accuracy, which is the number of dispersed points for the input target objects |
ReflectionObject | Returns the reflection object to reflect the input target objects |
RefractionIndex | Returns or sets the refraction index |
Resolution | Returns or sets the resolution type |
ReverseDir | Returns or sets whether the direction of reflection objects is reversed to determine their thickness |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetObject | Returns the target object to be reflected on the faces and/or planes the target object |
Thickness | Returns or sets the thickness of the reflection objects |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ReflectionDataBuilderResolutionType Enumeration | the resolution type |
Property Detail¶
EyePoint¶
-
ReflectionDataBuilder.
EyePoint
¶ Returns or sets the eye point
-------------------------------------
Getter Method
Signature
EyePoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EyePoint(eyePoint)
Parameters: eyePoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
IsReflectData¶
-
ReflectionDataBuilder.
IsReflectData
¶ Returns or sets whether to create reflection data as output or not
-------------------------------------
Getter Method
Signature
IsReflectData()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsReflectData(isReflectData)
Parameters: isReflectData (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
IsReflectTraceCurve¶
-
ReflectionDataBuilder.
IsReflectTraceCurve
¶ Returns or sets whether to create reflection trace curves as output or not
-------------------------------------
Getter Method
Signature
IsReflectTraceCurve()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsReflectTraceCurve(isReflectTraceCurve)
Parameters: isReflectTraceCurve (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
IsRefractData¶
-
ReflectionDataBuilder.
IsRefractData
¶ Returns or sets whether to create refraction data as output or not
-------------------------------------
Getter Method
Signature
IsRefractData()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsRefractData(isRefractData)
Parameters: isRefractData (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
IsRefractTraceCurve¶
-
ReflectionDataBuilder.
IsRefractTraceCurve
¶ Returns or sets whether to create refraction trace curves as output or not
-------------------------------------
Getter Method
Signature
IsRefractTraceCurve()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsRefractTraceCurve(isRefractTraceCurve)
Parameters: isRefractTraceCurve (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ReflectAccuracy¶
-
ReflectionDataBuilder.
ReflectAccuracy
¶ Returns or sets the customized reflection accuracy, which is the number of dispersed points for the input target objects
-------------------------------------
Getter Method
Signature
ReflectAccuracy()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReflectAccuracy(reflectAccuracy)
Parameters: reflectAccuracy (int) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ReflectionObject¶
-
ReflectionDataBuilder.
ReflectionObject
¶ Returns the reflection object to reflect the input target objects
-------------------------------------
Getter Method
Signature
ReflectionObject()
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
RefractionIndex¶
-
ReflectionDataBuilder.
RefractionIndex
¶ Returns or sets the refraction index
-------------------------------------
Getter Method
Signature
RefractionIndex()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RefractionIndex(refractionIndex)
Parameters: refractionIndex (float) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Resolution¶
-
ReflectionDataBuilder.
Resolution
¶ Returns or sets the resolution type
-------------------------------------
Getter Method
Signature
Resolution()
Returns: Return type: NXOpen.Features.VehicleDesign.ReflectionDataBuilderResolutionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Resolution(resolution)
Parameters: resolution ( NXOpen.Features.VehicleDesign.ReflectionDataBuilderResolutionType
) –New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ReverseDir¶
-
ReflectionDataBuilder.
ReverseDir
¶ Returns or sets whether the direction of reflection objects is reversed to determine their thickness
-------------------------------------
Getter Method
Signature
ReverseDir()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDir(reverseDir)
Parameters: reverseDir (bool) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
TargetObject¶
-
ReflectionDataBuilder.
TargetObject
¶ Returns the target object to be reflected on the faces and/or planes the target object
-------------------------------------
Getter Method
Signature
TargetObject()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
Thickness¶
-
ReflectionDataBuilder.
Thickness
¶ Returns or sets the thickness of the reflection objects
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Thickness(thickness)
Parameters: thickness (float) – New in version NX6.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
ReflectionDataBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.