ReflectionDataBuilderResolutionType Enumeration

NXOpen.Features.VehicleDesign.ReflectionDataBuilder.ResolutionType is an alias for NXOpen.Features.VehicleDesign.ReflectionDataBuilderResolutionType

class NXOpen.Features.VehicleDesign.ReflectionDataBuilderResolutionType

Bases: object

the resolution type

Enum Members

Enum Member Enum Member Description
Low
low
Medium
medium
High
high
Customized
user defined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.