VarsweepBuilder Class¶
-
class
NXOpen.Features.
VarsweepBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Variational Sweep feature builder.
It creates or edits VarSweep feature. To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateVarsweepBuilder()
Default values.
Property Value ConstantFittingSectionCount -1 PlayButtons.CurrentStep 0 PlayButtons.PlayModes PlayOnce PlayButtons.ScaleSpeed 1 PlayButtons.ScaleStep 0 PlayButtons.Speed 1 ReviewSection 0 New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AngularTolerance | Returns or sets the angle tolerance [degrees] |
BooleanOperation | Returns the boolean option |
ConstantFittingSectionCount | Returns or sets the constant fitting section count |
DistanceTolerance | Returns or sets the distance tolerance |
FeatureOptions | Returns the solid versus sheet body type option |
Limits | Returns the variational sweep limits |
List | Returns or sets the secondary section list |
MergeFacesOption | Returns or sets the merge faces option |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PathIncrement | Returns the path increment |
PlayButtons | Returns the play buttons builder |
ReProjectCurvesOption | Returns or sets the re-project curves option |
ReviewSection | Returns or sets the review section |
Section | Returns or sets the master section. |
SketchOnPathFeature | Returns the sketch on path |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
NewListItem | Create new list item @return |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngularTolerance¶
-
VarsweepBuilder.
AngularTolerance
¶ Returns or sets the angle tolerance [degrees]
-------------------------------------
Getter Method
Signature
AngularTolerance()
Returns: Return type: float New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
BooleanOperation¶
-
VarsweepBuilder.
BooleanOperation
¶ Returns the boolean option
-------------------------------------
Getter Method
Signature
BooleanOperation()
Returns: Return type: NXOpen.GeometricUtilities.BooleanOperation
New in version NX4.0.0.
License requirements: None.
ConstantFittingSectionCount¶
-
VarsweepBuilder.
ConstantFittingSectionCount
¶ Returns or sets the constant fitting section count
-------------------------------------
Getter Method
Signature
ConstantFittingSectionCount()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstantFittingSectionCount(constantFittingSectionCount)
Parameters: constantFittingSectionCount (int) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DistanceTolerance¶
-
VarsweepBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FeatureOptions¶
-
VarsweepBuilder.
FeatureOptions
¶ Returns the solid versus sheet body type option
-------------------------------------
Getter Method
Signature
FeatureOptions()
Returns: Return type: NXOpen.GeometricUtilities.FeatureOptions
New in version NX4.0.0.
License requirements: None.
Limits¶
-
VarsweepBuilder.
Limits
¶ Returns the variational sweep limits
-------------------------------------
Getter Method
Signature
Limits()
Returns: The variational sweep limits. Return type: NXOpen.GeometricUtilities.Limits
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
List¶
-
VarsweepBuilder.
List
¶ Returns or sets the secondary section list
-------------------------------------
Getter Method
Signature
List()
Returns: Return type: NXOpen.ObjectList
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
List(list)
Parameters: list ( NXOpen.ObjectList
) –New in version NX5.0.0.
License requirements: None.
MergeFacesOption¶
-
VarsweepBuilder.
MergeFacesOption
¶ Returns or sets the merge faces option
-------------------------------------
Getter Method
Signature
MergeFacesOption()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MergeFacesOption(mergeFacesOption)
Parameters: mergeFacesOption (bool) – New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
PathIncrement¶
-
VarsweepBuilder.
PathIncrement
¶ Returns the path increment
-------------------------------------
Getter Method
Signature
PathIncrement()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX11.0.0.
License requirements: None.
PlayButtons¶
-
VarsweepBuilder.
PlayButtons
¶ Returns the play buttons builder
-------------------------------------
Getter Method
Signature
PlayButtons()
Returns: Return type: NXOpen.GeometricUtilities.PlayButtonsBuilder
New in version NX11.0.0.
License requirements: None.
ReProjectCurvesOption¶
-
VarsweepBuilder.
ReProjectCurvesOption
¶ Returns or sets the re-project curves option
-------------------------------------
Getter Method
Signature
ReProjectCurvesOption()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReProjectCurvesOption(reProjectCurvesOption)
Parameters: reProjectCurvesOption (bool) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ReviewSection¶
-
VarsweepBuilder.
ReviewSection
¶ Returns or sets the review section
-------------------------------------
Getter Method
Signature
ReviewSection()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReviewSection(reviewSection)
Parameters: reviewSection (bool) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Section¶
-
VarsweepBuilder.
Section
¶ Returns or sets the master section.
Variational sweep accepts sections created ONLY on in the context of a Sketch on Path. Make sure this section is coming from sketch curves created using the sketch on path feature. Return code : 0 : no error, VARSWEEP_SKETCH_NOT_ON_PATH : on an error condition
-------------------------------------
Getter Method
Signature
Section()
Returns: Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Section(section)
Parameters: section ( NXOpen.Section
) – master sectionNew in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SketchOnPathFeature¶
-
VarsweepBuilder.
SketchOnPathFeature
¶ Returns the sketch on path
-------------------------------------
Getter Method
Signature
SketchOnPathFeature()
Returns: Return type: NXOpen.Features.Feature
New in version NX4.0.0.
License requirements: None.
Method Detail¶
NewListItem¶
-
VarsweepBuilder.
NewListItem
¶ Create new list item
Signature
NewListItem()
Returns: Return type: NXOpen.GeometricUtilities.SecondarySectionData
New in version NX5.0.0.
License requirements: None.
Validate¶
-
VarsweepBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.