BodyPreference |
Returns or sets the body type options |
Construction |
Returns or sets the construction options. |
CrossCurvesList |
Returns the cross curves list which is required. |
CrossSurfaceRebuildData |
Returns the cross surface rebuild data, NXOpen.GeometricUtilities.Rebuild . |
CrossTemplateString |
Returns the cross template curve. |
CurvatureTolerance |
Returns or sets the curvature tolerance. |
Emphasis |
Returns or sets the emphasis options. |
FirstCrossContinuity |
Returns the first cross continuity, NXOpen.GeometricUtilities.Continuity . |
FirstPrimaryContinuity |
Returns the first primary continuity, NXOpen.GeometricUtilities.Continuity . |
IntersectionTolerance |
Returns or sets the intersection tolerance. |
LastCrossContinuity |
Returns the last cross continuity, NXOpen.GeometricUtilities.Continuity . |
LastPrimaryContinuity |
Returns the last primary continuity, NXOpen.GeometricUtilities.Continuity . |
ParentFeatureInternal |
Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag |
Returns or sets the patch solution flag |
PatchSurfaceFilename |
Returns or sets the patch surface filename |
PositionTolerance |
Returns or sets the position tolerance. |
PrimaryCurvesList |
Returns the primary curves list which is required. |
PrimarySurfaceRebuildData |
Returns the primary surface rebuild data, NXOpen.GeometricUtilities.Rebuild . |
PrimaryTemplateString |
Returns the primary template curve. |
Spine |
Returns the spine. |
SurroundingPatchSurfaceFilename |
Returns or sets the surrounding patch surface filename |
Tag |
Returns the Tag for this object. |
TangentTolerance |
Returns or sets the tangent tolerance. |