ThroughCurveMeshBuilderEmphasisType Enumeration

NXOpen.Features.ThroughCurveMeshBuilder.EmphasisType is an alias for NXOpen.Features.ThroughCurveMeshBuilderEmphasisType

class NXOpen.Features.ThroughCurveMeshBuilderEmphasisType

Bases: object

This enum represents the Emphasis options.

Enum Members

Enum Member Enum Member Description
Both
Emphasis on both primary and cross strings.
Primary
Emphasis on primary strings.
Cross
Emphasis on cross strings.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.