MoveFaceBuilder Class¶
-
class
NXOpen.Features.
MoveFaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder for a move face feature, don’t use it until nx502.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateMoveFaceBuilder()
Default values.
Property Value Angle.Value 10.0 Distance.Value 10.0 (millimeters part), 0.4 (inches part) New in version NX5.0.2.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle for axis and angle option, don’t use it until nx502 |
Axis | Returns or sets the axis for axis and angle option, don’t use it until nx502 |
BlendFaces | Returns the face collector holding the all the recognized blend faces adjacent to face to move. |
Copy | Returns or sets the copy option for move face, don’t use it until nx502 |
Direction | Returns or sets the vector for direction and distance option, don’t use it until nx502 |
Distance | Returns the distance for direction and distance option, don’t use it until nx502 |
FromPoint | Returns or sets the from point in point to point option in move face, don’t use it until nx502 |
FromVector | Returns or sets the from vector in axis to axis option in move face, don’t use it until nx502 |
MoveFaceCollector | Returns the face collector holding the faces to move |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PivotPoint | Returns or sets the pivot point in axis to axis option in move face, don’t use it until nx502 |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ToPoint | Returns or sets the to point in point to point option in move face, don’t use it until nx502 |
ToVector | Returns or sets the to vector in axis to axis option in move face, don’t use it until nx502 |
Type | Returns or sets the type, don’t use it until nx502 |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MoveFaceBuilderTypes Enumeration | the move face types, don’t use it until nx502 |
Property Detail¶
Angle¶
-
MoveFaceBuilder.
Angle
¶ Returns the angle for axis and angle option, don’t use it until nx502
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
Axis¶
-
MoveFaceBuilder.
Axis
¶ Returns or sets the axis for axis and angle option, don’t use it until nx502
-------------------------------------
Getter Method
Signature
Axis()
Returns: Return type: NXOpen.Axis
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Axis(axis)
Parameters: axis ( NXOpen.Axis
) –New in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
BlendFaces¶
-
MoveFaceBuilder.
BlendFaces
¶ Returns the face collector holding the all the recognized blend faces adjacent to face to move.
It is auto recognized blends + user selected blends - user excluded blends, don’t use it until nx502
-------------------------------------
Getter Method
Signature
BlendFaces()
Returns: the adjacent blend faces builder Return type: NXOpen.ModlDirect.SelectBlend
New in version NX5.0.2.
License requirements: None.
Copy¶
-
MoveFaceBuilder.
Copy
¶ Returns or sets the copy option for move face, don’t use it until nx502
-------------------------------------
Getter Method
Signature
Copy()
Returns: Return type: bool New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Copy(copyOption)
Parameters: copyOption (bool) – New in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
Direction¶
-
MoveFaceBuilder.
Direction
¶ Returns or sets the vector for direction and distance option, don’t use it until nx502
-------------------------------------
Getter Method
Signature
Direction()
Returns: Return type: NXOpen.Direction
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction(direction)
Parameters: direction ( NXOpen.Direction
) –New in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
Distance¶
-
MoveFaceBuilder.
Distance
¶ Returns the distance for direction and distance option, don’t use it until nx502
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX5.0.2.
License requirements: None.
FromPoint¶
-
MoveFaceBuilder.
FromPoint
¶ Returns or sets the from point in point to point option in move face, don’t use it until nx502
-------------------------------------
Getter Method
Signature
FromPoint()
Returns: the from point Return type: NXOpen.Point
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FromPoint(fromPoint)
Parameters: fromPoint ( NXOpen.Point
) – the from pointNew in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
FromVector¶
-
MoveFaceBuilder.
FromVector
¶ Returns or sets the from vector in axis to axis option in move face, don’t use it until nx502
-------------------------------------
Getter Method
Signature
FromVector()
Returns: the from vector Return type: NXOpen.Direction
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FromVector(fromVector)
Parameters: fromVector ( NXOpen.Direction
) – the from vectorNew in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
MoveFaceCollector¶
-
MoveFaceBuilder.
MoveFaceCollector
¶ Returns the face collector holding the faces to move
-------------------------------------
Getter Method
Signature
MoveFaceCollector()
Returns: the move face collector Return type: NXOpen.ScCollector
New in version NX5.0.2.
License requirements: None.
PivotPoint¶
-
MoveFaceBuilder.
PivotPoint
¶ Returns or sets the pivot point in axis to axis option in move face, don’t use it until nx502
-------------------------------------
Getter Method
Signature
PivotPoint()
Returns: the pivot point Return type: NXOpen.Point
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PivotPoint(pivotPoint)
Parameters: pivotPoint ( NXOpen.Point
) – the pivot pointNew in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
ToPoint¶
-
MoveFaceBuilder.
ToPoint
¶ Returns or sets the to point in point to point option in move face, don’t use it until nx502
-------------------------------------
Getter Method
Signature
ToPoint()
Returns: the to point Return type: NXOpen.Point
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToPoint(toPoint)
Parameters: toPoint ( NXOpen.Point
) – the to pointNew in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
ToVector¶
-
MoveFaceBuilder.
ToVector
¶ Returns or sets the to vector in axis to axis option in move face, don’t use it until nx502
-------------------------------------
Getter Method
Signature
ToVector()
Returns: the to vector Return type: NXOpen.Direction
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToVector(toVector)
Parameters: toVector ( NXOpen.Direction
) – the to vectorNew in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
Type¶
-
MoveFaceBuilder.
Type
¶ Returns or sets the type, don’t use it until nx502
-------------------------------------
Getter Method
Signature
Type()
Returns: the move face type Return type: NXOpen.Features.MoveFaceBuilderTypes
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(moveType)
Parameters: moveType ( NXOpen.Features.MoveFaceBuilderTypes
) – the move face typeNew in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
MoveFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.