SelectBlend Class¶
-
class
NXOpen.ModlDirect.
SelectBlend
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.ModlDirect.SelectBlend
Allows user to specify blend faces.New in version NX5.0.2.
Properties¶
Property | Description |
---|---|
FaceCollector | Returns the blend faces collector. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ExcludeBlend | Exclude the user de-selected blend face |
IncludeBlend | Include the use selected blend face |
RecognizeBlends | Auto regonize the adjacent blends of input base faces |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FaceCollector¶
-
SelectBlend.
FaceCollector
¶ Returns the blend faces collector.
-------------------------------------
Getter Method
Signature
FaceCollector()
Returns: the blend face collector Return type: NXOpen.ScCollector
New in version NX5.0.2.
License requirements: None.
Method Detail¶
ExcludeBlend¶
-
SelectBlend.
ExcludeBlend
¶ Exclude the user de-selected blend face
Signature
ExcludeBlend(blendFace)
Parameters: blendFace ( NXOpen.Face
) – the blend face to excludeNew in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
IncludeBlend¶
-
SelectBlend.
IncludeBlend
¶ Include the use selected blend face
Signature
IncludeBlend(blendFace)
Parameters: blendFace ( NXOpen.Face
) – the blend face to includeNew in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
RecognizeBlends¶
-
SelectBlend.
RecognizeBlends
¶ Auto regonize the adjacent blends of input base faces
Signature
RecognizeBlends(baseFaces)
Parameters: baseFaces (list of NXOpen.Face
) – the base facesReturns: the adjacent blend faces Return type: list of NXOpen.Face
New in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
SelectBlend.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.