MoveFaceBuilderTypes Enumeration

NXOpen.Features.MoveFaceBuilder.Types is an alias for NXOpen.Features.MoveFaceBuilderTypes

class NXOpen.Features.MoveFaceBuilderTypes

Bases: object

the move face types, don’t use it until nx502

Enum Members

Enum Member Enum Member Description
TranslateDirectionAndDistance
Direction and Distance for moving the faces
TranslateBetweenTwoPoints
Move faces in the direction and distance defined by the two points
RotateAboutAxis
Move faces by rotating about an axis
RotateBetweenTwoAxes
Move faces by rotating the axis from the first to the second
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.