MatchedReferenceBuilder Class¶
-
class
NXOpen.Features.
MatchedReferenceBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Features.MatchedReferenceBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
MatchedEntity | Returns or sets the matched entity |
MatchedStatus | Returns or sets the matchedReference matched status |
ParentEntity | Returns the matchedReference parent entity |
ReverseDirection | Returns or sets the reverse direction |
Tag | Returns the Tag for this object. |
Type | Returns or sets the matchedReference type |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MatchedReferenceBuilderResolvedStatus Enumeration | Matched status |
MatchedReferenceBuilderTypes Enumeration | MatchedReference block type |
Property Detail¶
MatchedEntity¶
-
MatchedReferenceBuilder.
MatchedEntity
¶ Returns or sets the matched entity
-------------------------------------
Getter Method
Signature
MatchedEntity()
Returns: Return type: NXOpen.NXObject
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MatchedEntity(matchedEntity)
Parameters: matchedEntity ( NXOpen.NXObject
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
MatchedStatus¶
-
MatchedReferenceBuilder.
MatchedStatus
¶ Returns or sets the matchedReference matched status
-------------------------------------
Getter Method
Signature
MatchedStatus()
Returns: Return type: NXOpen.Features.MatchedReferenceBuilderResolvedStatus
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MatchedStatus(matchedStatus)
Parameters: matchedStatus ( NXOpen.Features.MatchedReferenceBuilderResolvedStatus
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ParentEntity¶
-
MatchedReferenceBuilder.
ParentEntity
¶ Returns the matchedReference parent entity
-------------------------------------
Getter Method
Signature
ParentEntity()
Returns: Return type: NXOpen.NXObject
New in version NX8.0.1.
License requirements: None.
ReverseDirection¶
-
MatchedReferenceBuilder.
ReverseDirection
¶ Returns or sets the reverse direction
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Type¶
-
MatchedReferenceBuilder.
Type
¶ Returns or sets the matchedReference type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.MatchedReferenceBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.MatchedReferenceBuilderTypes
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
MatchedReferenceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.