MatchedReferenceBuilderTypes Enumeration

NXOpen.Features.MatchedReferenceBuilder.Types is an alias for NXOpen.Features.MatchedReferenceBuilderTypes

class NXOpen.Features.MatchedReferenceBuilderTypes

Bases: object

MatchedReference block type

Enum Members

Enum Member Enum Member Description
Curve
single curve or edge
Face
single face or datum plane
CurveCollector
curve collector or edge collector
FaceCollector
face collector
Section
section
Point
point
Vector
vector
Object
general geometry such as the target body and the tool body for copying unite feature
BodyCollector
body collector
Csys
csys
Plane
plane
Axis
axis
Undefined
default type for feature name lable
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.