MatchedReferenceBuilderResolvedStatus Enumeration

NXOpen.Features.MatchedReferenceBuilder.ResolvedStatus is an alias for NXOpen.Features.MatchedReferenceBuilderResolvedStatus

class NXOpen.Features.MatchedReferenceBuilderResolvedStatus

Bases: object

Matched status

Enum Members

Enum Member Enum Member Description
Initial
initial state
Unresolved
user unresolved
BySystem
system automatic resolve
ByUser
resolve by user
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.