CustomFeatureDataCollection Class¶
-
class
NXOpen.Features.
CustomFeatureDataCollection
¶ Bases:
object
This class contains the factory method for creating custom feature data object.
To obtain an instance of this class, refer to
NXOpen.Features.FeatureCollection
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateData | Creates an Features.CustomFeatureData with parameters. |
Method Detail¶
CreateData¶
-
CustomFeatureDataCollection.
CreateData
¶ Creates an
Features.CustomFeatureData
with parameters.Signature
CreateData(cfclass, attrs)
Parameters: - cfclass (
NXOpen.Features.CustomFeatureClass
) – - attrs (list of
NXOpen.Features.CustomAttribute
) –
Returns: custom feature data
Return type: New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- cfclass (