CustomAttribute Class¶
-
class
NXOpen.Features.
CustomAttribute
¶ Bases:
NXOpen.TransientObject
Represents a
Features.CustomAttribute
classThis is an abstract base class of all the types of attributes.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns or sets the custom attribute name |
TypeValue | Returns the custom attribute type value |
Methods¶
Method | Description |
---|---|
AddProperty | The custom attribute add property |
Dispose | Frees the memory associated with this object. |
GetProperties | The custom attribute get all properties @return |
HasProperty | The custom attribute does property exist on attribute @return |
RemoveProperty | The custom attribute remove property |
Enumerations¶
CustomAttributeProperty Enumeration | Specifies custom attribute type. |
CustomAttributeType Enumeration | Specifies custom attribute type. |
Property Detail¶
Name¶
-
CustomAttribute.
Name
¶ Returns or sets the custom attribute name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
Name(attributeName)
Parameters: attributeName (str) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TypeValue¶
-
CustomAttribute.
TypeValue
¶ Returns the custom attribute type value
-------------------------------------
Getter Method
Signature
TypeValue()
Returns: Return type: NXOpen.Features.CustomAttributeType
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
AddProperty¶
-
CustomAttribute.
AddProperty
¶ The custom attribute add property
Signature
AddProperty(attributeProperty)
Parameters: attributeProperty ( NXOpen.Features.CustomAttributeProperty
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Dispose¶
-
CustomAttribute.
Dispose
¶ Frees the memory associated with this object.
After invocation of this method, the object is no longer valid.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetProperties¶
-
CustomAttribute.
GetProperties
¶ The custom attribute get all properties
Signature
GetProperties()
Returns: Return type: list of NXOpen.Features.CustomAttributeProperty
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
HasProperty¶
-
CustomAttribute.
HasProperty
¶ The custom attribute does property exist on attribute
Signature
HasProperty(attributeProperty)
Parameters: attributeProperty ( NXOpen.Features.CustomAttributeProperty
) –Returns: Return type: bool New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveProperty¶
-
CustomAttribute.
RemoveProperty
¶ The custom attribute remove property
Signature
RemoveProperty(attributeProperty)
Parameters: attributeProperty ( NXOpen.Features.CustomAttributeProperty
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)