BridgeSurfaceBuilder Class¶
-
class
NXOpen.Features.
BridgeSurfaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.BridgeSurface
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateBridgeSurfaceBuilder()
Default values.
Property Value EdgeFlowDirection.FlowDirectionType NotSpecified FirstEdgeContinuity.ContinuityType G1 FirstEdgeRange.AnchorPosition Start IsFirstEdgeLimitEndToEnd 0 IsSecondEdgeLimitEndToEnd 0 SecondEdgeContinuity.ContinuityType G1 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
EdgeFlowDirection | Returns the flow direction. |
EdgeTangentMagnitude | Returns the edge tangent magnitude |
FirstEdgeContinuity | Returns the first edge continuity |
FirstEdgeOffset | Returns the first edge offset |
FirstEdgeRange | Returns the first edge range |
FirstEdgeSelection | Returns the first edge selection |
G0Tolerance | Returns or sets the g0 tolerance |
G1Tolerance | Returns or sets the g1 tolerance |
G2Tolerance | Returns or sets the g2 tolerance |
IsEndHandlesLinked | Returns or sets the flag indicating if the end handles are linked |
IsFirstEdgeContinuityReversed | Returns or sets the flag indicating if continuity direction at first edge is reversed |
IsFirstEdgeLimitEndToEnd | Returns or sets the flag indicating if the first edge limit is end to end |
IsFirstEdgeReversed | Returns or sets the flag indicating if the first edge direction is reversed |
IsSecondEdgeContinuityReversed | Returns or sets the flag indicating if continuity direction at second edge is reversed |
IsSecondEdgeLimitEndToEnd | Returns or sets the flag indicating if the second edge limit is end to end |
IsSecondEdgeReversed | Returns or sets the flag indicating if the second edge direction is reversed |
IsStartHandlesLinked | Returns or sets the flag indicating if the start handles are linked |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Rebuild | Returns the surface rebuild data |
SecondEdgeContinuity | Returns the second edge continuity |
SecondEdgeOffset | Returns the second edge offset |
SecondEdgeRange | Returns the second edge range |
SecondEdgeSelection | Returns the second edge selection |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
ConstructSurfaceBoundaryCurve | Constructs bridge surface boundary curve |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EdgeFlowDirection¶
-
BridgeSurfaceBuilder.
EdgeFlowDirection
¶ Returns the flow direction.
See
NXOpen.GeometricUtilities.FlowDirection
for details.-------------------------------------
Getter Method
Signature
EdgeFlowDirection()
Returns: Return type: NXOpen.GeometricUtilities.FlowDirection
New in version NX8.0.0.
License requirements: None.
EdgeTangentMagnitude¶
-
BridgeSurfaceBuilder.
EdgeTangentMagnitude
¶ Returns the edge tangent magnitude
-------------------------------------
Getter Method
Signature
EdgeTangentMagnitude()
Returns: Return type: NXOpen.GeometricUtilities.TangentMagnitudeBuilder
New in version NX8.0.0.
License requirements: None.
FirstEdgeContinuity¶
-
BridgeSurfaceBuilder.
FirstEdgeContinuity
¶ Returns the first edge continuity
-------------------------------------
Getter Method
Signature
FirstEdgeContinuity()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX8.0.0.
License requirements: None.
FirstEdgeOffset¶
-
BridgeSurfaceBuilder.
FirstEdgeOffset
¶ Returns the first edge offset
-------------------------------------
Getter Method
Signature
FirstEdgeOffset()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.0.0.
License requirements: None.
FirstEdgeRange¶
-
BridgeSurfaceBuilder.
FirstEdgeRange
¶ Returns the first edge range
-------------------------------------
Getter Method
Signature
FirstEdgeRange()
Returns: Return type: NXOpen.GeometricUtilities.CurveRangeBuilder
New in version NX8.0.0.
License requirements: None.
FirstEdgeSelection¶
-
BridgeSurfaceBuilder.
FirstEdgeSelection
¶ Returns the first edge selection
-------------------------------------
Getter Method
Signature
FirstEdgeSelection()
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.0.0.
License requirements: None.
G0Tolerance¶
-
BridgeSurfaceBuilder.
G0Tolerance
¶ Returns or sets the g0 tolerance
-------------------------------------
Getter Method
Signature
G0Tolerance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G0Tolerance(g0Tolerance)
Parameters: g0Tolerance (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
G1Tolerance¶
-
BridgeSurfaceBuilder.
G1Tolerance
¶ Returns or sets the g1 tolerance
-------------------------------------
Getter Method
Signature
G1Tolerance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G1Tolerance(g1Tolerance)
Parameters: g1Tolerance (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
G2Tolerance¶
-
BridgeSurfaceBuilder.
G2Tolerance
¶ Returns or sets the g2 tolerance
-------------------------------------
Getter Method
Signature
G2Tolerance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G2Tolerance(g2Tolerance)
Parameters: g2Tolerance (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsEndHandlesLinked¶
-
BridgeSurfaceBuilder.
IsEndHandlesLinked
¶ Returns or sets the flag indicating if the end handles are linked
-------------------------------------
Getter Method
Signature
IsEndHandlesLinked()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsEndHandlesLinked(isEndHandlesLinked)
Parameters: isEndHandlesLinked (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsFirstEdgeContinuityReversed¶
-
BridgeSurfaceBuilder.
IsFirstEdgeContinuityReversed
¶ Returns or sets the flag indicating if continuity direction at first edge is reversed
-------------------------------------
Getter Method
Signature
IsFirstEdgeContinuityReversed()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsFirstEdgeContinuityReversed(isFirstEdgeContinuityReversed)
Parameters: isFirstEdgeContinuityReversed (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsFirstEdgeLimitEndToEnd¶
-
BridgeSurfaceBuilder.
IsFirstEdgeLimitEndToEnd
¶ Returns or sets the flag indicating if the first edge limit is end to end
-------------------------------------
Getter Method
Signature
IsFirstEdgeLimitEndToEnd()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsFirstEdgeLimitEndToEnd(isFirstEdgeLimitEndToEnd)
Parameters: isFirstEdgeLimitEndToEnd (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsFirstEdgeReversed¶
-
BridgeSurfaceBuilder.
IsFirstEdgeReversed
¶ Returns or sets the flag indicating if the first edge direction is reversed
-------------------------------------
Getter Method
Signature
IsFirstEdgeReversed()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsFirstEdgeReversed(isFirstEdgeReversed)
Parameters: isFirstEdgeReversed (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsSecondEdgeContinuityReversed¶
-
BridgeSurfaceBuilder.
IsSecondEdgeContinuityReversed
¶ Returns or sets the flag indicating if continuity direction at second edge is reversed
-------------------------------------
Getter Method
Signature
IsSecondEdgeContinuityReversed()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSecondEdgeContinuityReversed(isSecondEdgeContinuityReversed)
Parameters: isSecondEdgeContinuityReversed (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsSecondEdgeLimitEndToEnd¶
-
BridgeSurfaceBuilder.
IsSecondEdgeLimitEndToEnd
¶ Returns or sets the flag indicating if the second edge limit is end to end
-------------------------------------
Getter Method
Signature
IsSecondEdgeLimitEndToEnd()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSecondEdgeLimitEndToEnd(isSecondEdgeLimitEndToEnd)
Parameters: isSecondEdgeLimitEndToEnd (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsSecondEdgeReversed¶
-
BridgeSurfaceBuilder.
IsSecondEdgeReversed
¶ Returns or sets the flag indicating if the second edge direction is reversed
-------------------------------------
Getter Method
Signature
IsSecondEdgeReversed()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSecondEdgeReversed(isSecondEdgeReversed)
Parameters: isSecondEdgeReversed (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsStartHandlesLinked¶
-
BridgeSurfaceBuilder.
IsStartHandlesLinked
¶ Returns or sets the flag indicating if the start handles are linked
-------------------------------------
Getter Method
Signature
IsStartHandlesLinked()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsStartHandlesLinked(isStartHandlesLinked)
Parameters: isStartHandlesLinked (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Rebuild¶
-
BridgeSurfaceBuilder.
Rebuild
¶ Returns the surface rebuild data
-------------------------------------
Getter Method
Signature
Rebuild()
Returns: Return type: NXOpen.GeometricUtilities.Rebuild
New in version NX8.0.0.
License requirements: None.
SecondEdgeContinuity¶
-
BridgeSurfaceBuilder.
SecondEdgeContinuity
¶ Returns the second edge continuity
-------------------------------------
Getter Method
Signature
SecondEdgeContinuity()
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX8.0.0.
License requirements: None.
SecondEdgeOffset¶
-
BridgeSurfaceBuilder.
SecondEdgeOffset
¶ Returns the second edge offset
-------------------------------------
Getter Method
Signature
SecondEdgeOffset()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.0.0.
License requirements: None.
SecondEdgeRange¶
-
BridgeSurfaceBuilder.
SecondEdgeRange
¶ Returns the second edge range
-------------------------------------
Getter Method
Signature
SecondEdgeRange()
Returns: Return type: NXOpen.GeometricUtilities.CurveRangeBuilder
New in version NX8.0.0.
License requirements: None.
SecondEdgeSelection¶
-
BridgeSurfaceBuilder.
SecondEdgeSelection
¶ Returns the second edge selection
-------------------------------------
Getter Method
Signature
SecondEdgeSelection()
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.0.0.
License requirements: None.
Method Detail¶
ConstructSurfaceBoundaryCurve¶
-
BridgeSurfaceBuilder.
ConstructSurfaceBoundaryCurve
¶ Constructs bridge surface boundary curve
Signature
ConstructSurfaceBoundaryCurve(startBoundary)
Parameters: startBoundary (bool) – True if start boundary and false if end boundary New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
BridgeSurfaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.