FacetBodyFromBodyBuilder Class¶
-
class
NXOpen.Facet.
FacetBodyFromBodyBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Facet.FacetBodyFromBodyBuilder
builder.It converts the selected analytic bodies to NX convergent bodies bodies. The original inputs are deleted.
To create a new instance of this class, use
NXOpen.Facet.FacetModelingCollection.CreateFacetBodyFromBodyBuilder()
Default values.
Property Value MaximumDeviation 0.1 (millimeters part), 0.005 (inches part) OriginalBodyOption Hide OutputType NXFacetBody New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
MaximumDeviation | Returns or sets the maximum deviation |
NonFacetedBodiesToConvert | Returns the input non-faceted bodies to convert |
OriginalBodyOption | Returns or sets the original body option of enum |
OutputType | Returns or sets the output of the type of enum |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FacetBodyFromBodyBuilderOriginalBodyOptions Enumeration | These options represent the options for handling original body: Keep, Hide, Delete |
FacetBodyFromBodyBuilderOutputTypes Enumeration | These options represent the type of output body |
Property Detail¶
MaximumDeviation¶
-
FacetBodyFromBodyBuilder.
MaximumDeviation
¶ Returns or sets the maximum deviation
-------------------------------------
Getter Method
Signature
MaximumDeviation()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumDeviation(maximumDeviation)
Parameters: maximumDeviation (float) – New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
NonFacetedBodiesToConvert¶
-
FacetBodyFromBodyBuilder.
NonFacetedBodiesToConvert
¶ Returns the input non-faceted bodies to convert
-------------------------------------
Getter Method
Signature
NonFacetedBodiesToConvert()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX10.0.0.
License requirements: None.
OriginalBodyOption¶
-
FacetBodyFromBodyBuilder.
OriginalBodyOption
¶ Returns or sets the original body option of enum
-------------------------------------
Getter Method
Signature
OriginalBodyOption()
Returns: Return type: NXOpen.Facet.FacetBodyFromBodyBuilderOriginalBodyOptions
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OriginalBodyOption(enumOriginalBodyOption)
Parameters: enumOriginalBodyOption ( NXOpen.Facet.FacetBodyFromBodyBuilderOriginalBodyOptions
) –New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
OutputType¶
-
FacetBodyFromBodyBuilder.
OutputType
¶ Returns or sets the output of the type of enum
-------------------------------------
Getter Method
Signature
OutputType()
Returns: Return type: NXOpen.Facet.FacetBodyFromBodyBuilderOutputTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputType(enumOutputType)
Parameters: enumOutputType ( NXOpen.Facet.FacetBodyFromBodyBuilderOutputTypes
) –New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
Validate¶
-
FacetBodyFromBodyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.