FacetBodyFromBodyBuilderOriginalBodyOptions Enumeration¶
NXOpen.Facet.FacetBodyFromBodyBuilder.OriginalBodyOptions is an alias for NXOpen.Facet.FacetBodyFromBodyBuilderOriginalBodyOptions
-
class
NXOpen.Facet.
FacetBodyFromBodyBuilderOriginalBodyOptions
¶ Bases:
object
These options represent the options for handling original body: Keep, Hide, Delete
Enum Members
Enum Member Enum Member Description Keep Keep original bodyHide Hide original bodyDelete Delete original body-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-