FacetBodyFromBodyBuilderOutputTypes Enumeration¶
NXOpen.Facet.FacetBodyFromBodyBuilder.OutputTypes is an alias for NXOpen.Facet.FacetBodyFromBodyBuilderOutputTypes
-
class
NXOpen.Facet.
FacetBodyFromBodyBuilderOutputTypes
¶ Bases:
object
These options represent the type of output body
Enum Members
Enum Member Enum Member Description NXFacetBody Convert to NX Facet BodiesConvergentBody Convert To Convergent bodiesJTFacetBody Convert To JT Facet bodies-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-