UncutRegionsBuilder Class¶
-
class
NXOpen.Die.
UncutRegionsBuilder
¶ Bases:
NXOpen.Builder
Calculates the uncut regions of a curve given a radius value for the cut tool.
To create a new instance of this class, use
NXOpen.Die.DieCollection.CreateUncutRegionsBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Curves | Returns the curves to check for uncut regions. |
Results | Returns or sets the side of the curve to show the results. |
Tag | Returns the Tag for this object. |
ToolAxis | Returns or sets the tool axis. |
ToolSize | Returns the expression that contains the tool radius. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ReverseSide | Reverse the tool side |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
UncutRegionsBuilderResultsType Enumeration | Indicates which side of curve to check |
Property Detail¶
Curves¶
-
UncutRegionsBuilder.
Curves
¶ Returns the curves to check for uncut regions.
-------------------------------------
Getter Method
Signature
Curves()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
Results¶
-
UncutRegionsBuilder.
Results
¶ Returns or sets the side of the curve to show the results.
-------------------------------------
Getter Method
Signature
Results()
Returns: Return type: NXOpen.Die.UncutRegionsBuilderResultsType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Results(results)
Parameters: results ( NXOpen.Die.UncutRegionsBuilderResultsType
) –New in version NX7.5.0.
License requirements: None.
ToolAxis¶
-
UncutRegionsBuilder.
ToolAxis
¶ Returns or sets the tool axis.
-------------------------------------
Getter Method
Signature
ToolAxis()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolAxis(toolAxis)
Parameters: toolAxis ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: None.
ToolSize¶
-
UncutRegionsBuilder.
ToolSize
¶ Returns the expression that contains the tool radius.
-------------------------------------
Getter Method
Signature
ToolSize()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Method Detail¶
ReverseSide¶
-
UncutRegionsBuilder.
ReverseSide
¶ Reverse the tool side
Signature
ReverseSide()
New in version NX7.5.0.
License requirements: None.
Validate¶
-
UncutRegionsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.