UncutRegionsBuilderResultsType Enumeration

NXOpen.Die.UncutRegionsBuilder.ResultsType is an alias for NXOpen.Die.UncutRegionsBuilderResultsType

class NXOpen.Die.UncutRegionsBuilderResultsType

Bases: object

Indicates which side of curve to check

Enum Members

Enum Member Enum Member Description
OneSide
Find uncut regions on one side only
BothSides
Find uncut regions on both sides of curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.