OutputCurvesBuilder Class

class NXOpen.Die.OutputCurvesBuilder

Bases: NXOpen.Features.FeatureBuilder

Represents an output curves feature builder.

This is an abstract class, and cannot be created.

New in version NX4.0.1.

Properties

Property Description
AngleTolerance Returns or sets the angle tolerance.
DistanceTolerance Returns or sets the distance tolerance.
FirstLimitPoint Returns or sets the first limit point.
LastLimitPoint Returns or sets the last limit point.
OffsetDistance Returns or sets the offset distance
ParentFeatureInternal Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal
PatchSolutionFlag Returns or sets the patch solution flag
PatchSurfaceFilename Returns or sets the patch surface filename
ReferenceFeature Returns or sets the reference feature - must be either a die section or form task feature
ReferencePoint Returns or sets the reference point.
SmoothTolerance Returns or sets the tolerance used for cubic or quintic smoothing.
SmoothType Returns or sets the smooth type
SurroundingPatchSurfaceFilename Returns or sets the surrounding patch surface filename
Tag Returns the Tag for this object.
TrimCurveCreateType Returns or sets the trim curve creation type
TrimCurveType Returns or sets the trim curve type.
TrimOutputCurveType Returns or sets the trim curve output type

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
CommitFeature Commits the feature parameters and creates the feature @return
CreateNonAssociative Creates the output curve without a feature.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetFeature Returns the feature currently being edited by this builder.
GetObject Returns the object currently being edited by this builder.
HideInternalParentFeatureAfterEdit Re-suppress an internal parent feature (a slave feature) after it has been edited.
SetParentFeatureInternal Set the parent features which would be internal or slaves to the feature being created or commited
ShowInternalParentFeatureForEdit Unsuppress an internal parent feature (a slave feature) so it can be edited.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
UnsetParentFeatureInternal Set the internal parent feature of the feature being edited to external
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

OutputCurvesBuilderSmoothTypes Enumeration Settings for the curve smoothing type.
OutputCurvesBuilderTrimCurveCreateTypes Enumeration Settings for the trim curve creation type.
OutputCurvesBuilderTrimCurveTypes Enumeration Settings for the trim curve type.
OutputCurvesBuilderTrimOutputCurveTypes Enumeration Settings for the trim curve output type.

Property Detail

AngleTolerance

OutputCurvesBuilder.AngleTolerance

Returns or sets the angle tolerance.

-------------------------------------

Getter Method

Signature AngleTolerance()

Returns:
Return type:float

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature AngleTolerance(angleTolerance)

Parameters:angleTolerance (float) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

DistanceTolerance

OutputCurvesBuilder.DistanceTolerance

Returns or sets the distance tolerance.

-------------------------------------

Getter Method

Signature DistanceTolerance()

Returns:
Return type:float

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature DistanceTolerance(distanceTolerance)

Parameters:distanceTolerance (float) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

FirstLimitPoint

OutputCurvesBuilder.FirstLimitPoint

Returns or sets the first limit point.

-------------------------------------

Getter Method

Signature FirstLimitPoint()

Returns:
Return type:NXOpen.Point3d

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature FirstLimitPoint(firstLimitPoint)

Parameters:firstLimitPoint (NXOpen.Point3d) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

LastLimitPoint

OutputCurvesBuilder.LastLimitPoint

Returns or sets the last limit point.

-------------------------------------

Getter Method

Signature LastLimitPoint()

Returns:
Return type:NXOpen.Point3d

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature LastLimitPoint(lastLimitPoint)

Parameters:lastLimitPoint (NXOpen.Point3d) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

OffsetDistance

OutputCurvesBuilder.OffsetDistance

Returns or sets the offset distance

-------------------------------------

Getter Method

Signature OffsetDistance()

Returns:each non-trim offset curve will be output by this distance
Return type:float

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature OffsetDistance(offsetDistance)

Parameters:offsetDistance (float) – each non-trim offset curve will be output by this distance

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

ReferenceFeature

OutputCurvesBuilder.ReferenceFeature

Returns or sets the reference feature - must be either a die section or form task feature

-------------------------------------

Getter Method

Signature ReferenceFeature()

Returns:
Return type:NXOpen.Features.Feature

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature ReferenceFeature(referenceFeature)

Parameters:referenceFeature (NXOpen.Features.Feature) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

ReferencePoint

OutputCurvesBuilder.ReferencePoint

Returns or sets the reference point.

-------------------------------------

Getter Method

Signature ReferencePoint()

Returns:Reference point indicating which output curve you want
Return type:NXOpen.Point3d

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature ReferencePoint(referencePoint)

Parameters:referencePoint (NXOpen.Point3d) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

SmoothTolerance

OutputCurvesBuilder.SmoothTolerance

Returns or sets the tolerance used for cubic or quintic smoothing.

-------------------------------------

Getter Method

Signature SmoothTolerance()

Returns:
Return type:float

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature SmoothTolerance(smoothTolerance)

Parameters:smoothTolerance (float) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

SmoothType

OutputCurvesBuilder.SmoothType

Returns or sets the smooth type

-------------------------------------

Getter Method

Signature SmoothType()

Returns:
Return type:NXOpen.Die.OutputCurvesBuilderSmoothTypes

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature SmoothType(smoothType)

Parameters:smoothType (NXOpen.Die.OutputCurvesBuilderSmoothTypes) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

TrimCurveCreateType

OutputCurvesBuilder.TrimCurveCreateType

Returns or sets the trim curve creation type

-------------------------------------

Getter Method

Signature TrimCurveCreateType()

Returns:
Return type:NXOpen.Die.OutputCurvesBuilderTrimCurveCreateTypes

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature TrimCurveCreateType(trimCurveType)

Parameters:trimCurveType (NXOpen.Die.OutputCurvesBuilderTrimCurveCreateTypes) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

TrimCurveType

OutputCurvesBuilder.TrimCurveType

Returns or sets the trim curve type.

Needs to be set before reference point

-------------------------------------

Getter Method

Signature TrimCurveType()

Returns:
Return type:NXOpen.Die.OutputCurvesBuilderTrimCurveTypes

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature TrimCurveType(trimCurveType)

Parameters:trimCurveType (NXOpen.Die.OutputCurvesBuilderTrimCurveTypes) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

TrimOutputCurveType

OutputCurvesBuilder.TrimOutputCurveType

Returns or sets the trim curve output type

-------------------------------------

Getter Method

Signature TrimOutputCurveType()

Returns:
Return type:NXOpen.Die.OutputCurvesBuilderTrimOutputCurveTypes

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

-------------------------------------

Setter Method

Signature TrimOutputCurveType(trimCurveOutputType)

Parameters:trimCurveOutputType (NXOpen.Die.OutputCurvesBuilderTrimOutputCurveTypes) –

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

Method Detail

CreateNonAssociative

OutputCurvesBuilder.CreateNonAssociative

Creates the output curve without a feature.

Signature CreateNonAssociative()

Returns:output curves
Return type:list of NXOpen.ICurve

New in version NX4.0.1.

License requirements: die_engineering (“DIE ENGINEERING”)

Validate

OutputCurvesBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.