OutputCurvesBuilderTrimCurveCreateTypes Enumeration

NXOpen.Die.OutputCurvesBuilder.TrimCurveCreateTypes is an alias for NXOpen.Die.OutputCurvesBuilderTrimCurveCreateTypes

class NXOpen.Die.OutputCurvesBuilderTrimCurveCreateTypes

Bases: object

Settings for the trim curve creation type.

New in version NX4.0.1.

Enum Members

Enum Member Enum Member Description
Section
Section.
Surface
Surface.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.