OutputCurvesBuilderTrimOutputCurveTypes Enumeration

NXOpen.Die.OutputCurvesBuilder.TrimOutputCurveTypes is an alias for NXOpen.Die.OutputCurvesBuilderTrimOutputCurveTypes

class NXOpen.Die.OutputCurvesBuilderTrimOutputCurveTypes

Bases: object

Settings for the trim curve output type.

New in version NX4.0.1.

Enum Members

Enum Member Enum Member Description
Geometric
Geometric.
Corrected
Corrected.
Both
Both geometric and corrected.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.