CannedAnnotationBuilder Class¶
-
class
NXOpen.Diagramming.
CannedAnnotationBuilder
¶ Bases:
NXOpen.Builder
Represents a CannedAnnotationBuilder.
To create a new instance of this class, use
NXOpen.Diagramming.DiagrammingManager.CreateCannedAnnotationBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AnnotationBuilder | Returns the annotation of this canned annotation. |
LeaderLines | Returns the list of the leader lines. |
Tag | Returns the Tag for this object. |
TextBoxIndent | Returns or sets the indent value of the text box in the canned annotation. |
TextBoxModifiable | Returns or sets the flag that indicates if the text box in the canned annotation is modifiable. |
TextBoxShadowBox | Returns or sets the flag that indicates if the text box in the canned annotation has shadow box. |
TextBoxWrappable | Returns or sets the flag that indicates if the text box in the canned annotation is wrappable. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateLeaderLine | Create a new NXOpen.Diagramming.LeaderLineBuilder builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
Inherit | Inherit. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CannedAnnotationBuilderInheritOption Enumeration | Represents the inherit option. |
Property Detail¶
AnnotationBuilder¶
-
CannedAnnotationBuilder.
AnnotationBuilder
¶ Returns the annotation of this canned annotation.
-------------------------------------
Getter Method
Signature
AnnotationBuilder()
Returns: Return type: NXOpen.Diagramming.AnnotationBuilder
New in version NX10.0.0.
License requirements: None.
LeaderLines¶
-
CannedAnnotationBuilder.
LeaderLines
¶ Returns the list of the leader lines.
-------------------------------------
Getter Method
Signature
LeaderLines()
Returns: Return type: NXOpen.Diagramming.LeaderLineBuilderList
New in version NX10.0.0.
License requirements: None.
TextBoxIndent¶
-
CannedAnnotationBuilder.
TextBoxIndent
¶ Returns or sets the indent value of the text box in the canned annotation.
-------------------------------------
Getter Method
Signature
TextBoxIndent()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextBoxIndent(indent)
Parameters: indent (int) – New in version NX10.0.0.
License requirements: None.
TextBoxModifiable¶
-
CannedAnnotationBuilder.
TextBoxModifiable
¶ Returns or sets the flag that indicates if the text box in the canned annotation is modifiable.
-------------------------------------
Getter Method
Signature
TextBoxModifiable()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextBoxModifiable(isModifiable)
Parameters: isModifiable (bool) – New in version NX10.0.0.
License requirements: None.
TextBoxShadowBox¶
-
CannedAnnotationBuilder.
TextBoxShadowBox
¶ Returns or sets the flag that indicates if the text box in the canned annotation has shadow box.
-------------------------------------
Getter Method
Signature
TextBoxShadowBox()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextBoxShadowBox(isShadowBox)
Parameters: isShadowBox (bool) – New in version NX10.0.0.
License requirements: None.
TextBoxWrappable¶
-
CannedAnnotationBuilder.
TextBoxWrappable
¶ Returns or sets the flag that indicates if the text box in the canned annotation is wrappable.
-------------------------------------
Getter Method
Signature
TextBoxWrappable()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextBoxWrappable(isWrappable)
Parameters: isWrappable (bool) – New in version NX10.0.0.
License requirements: None.
Method Detail¶
CreateLeaderLine¶
-
CannedAnnotationBuilder.
CreateLeaderLine
¶ Create a new
NXOpen.Diagramming.LeaderLineBuilder
builder.Signature
CreateLeaderLine()
Returns: Return type: NXOpen.Diagramming.LeaderLineBuilder
New in version NX10.0.0.
License requirements: None.
Inherit¶
-
CannedAnnotationBuilder.
Inherit
¶ Inherit.
Signature
Inherit(inheritOption, annotation)
Parameters: - inheritOption (
NXOpen.Diagramming.CannedAnnotationBuilderInheritOption
) – - annotation (
NXOpen.Diagramming.Annotation
) –
New in version NX11.0.0.
License requirements: None.
- inheritOption (
Validate¶
-
CannedAnnotationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.