CannedAnnotationBuilderInheritOption Enumeration¶
NXOpen.Diagramming.CannedAnnotationBuilder.InheritOption is an alias for NXOpen.Diagramming.CannedAnnotationBuilderInheritOption
-
class
NXOpen.Diagramming.
CannedAnnotationBuilderInheritOption
¶ Bases:
object
Represents the inherit option.
New in version NX11.0.0.
Enum Members
Enum Member Enum Member Description Preferences Setting the inherit from preferences optionCustomerDefaults Setting the inherit from customer defaults optionSelection Setting the inherit from selection option-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-