LeaderLineBuilder Class¶
-
class
NXOpen.Diagramming.
LeaderLineBuilder
¶ Bases:
NXOpen.Diagramming.SheetElementBuilder
Represents a LeaderLineBuilder.
To create a new instance of this class, use
NXOpen.Diagramming.LeaderLineCollection.CreateLeaderLineBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ArrowType | Returns or sets the arrow type of the end arrow |
Height | Returns or sets the height. |
HeightPolicy | Returns or sets the height policy. |
Internal | Returns the flag that indicates if the sheet element is internal. |
Label | Returns the label of this sheet element. |
LabelName | Returns or sets the label name of this sheet element. |
Location | Returns the location of the sheet element relative to another sheet element. |
LocationStyle | Returns or sets the location style. |
MirrorX | Returns or sets the sheet element to Mirror along the X axis. |
MirrorY | Returns or sets the sheet element to Mirror along the Y axis. |
Owner | Returns or sets the owning sheet element. |
OwningSheet | Returns the owning sheet. |
ResizeOption | Returns or sets the resize option of the sheet element |
Rotation | Returns or sets the rotation angle that is counter clockwise and relative to the owner. |
SourceElement | Returns the source element that records which sheet element it is a copy of. |
StubLength | Returns or sets the stub length of this leader line. |
StubSides | Returns or sets the stub sides of this leader line. |
Tag | Returns the Tag for this object. |
UpToDate | Returns the flag that indicates if the sheet element is up to date. |
VerticalAlignment | Returns or sets the vertical alignment option. |
Visible | Returns the flag that indicates if the sheet element is visible. |
Width | Returns or sets the width. |
WidthPolicy | Returns or sets the width policy. |
NXOpen.Diagramming.SheetElementBuilder.X | Returns or sets the absolute x coordinate. |
NXOpen.Diagramming.SheetElementBuilder.Y | Returns or sets the absolute y coordinate. |
ZDepth | Returns or sets the Z depth. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAllowedTransformations | Get the allowed transformations of the sheet element. |
GetBendPoints | Get bending points for polyline to render the leader line. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetMinNodeSize | Gets the minimum node size values |
GetObject | Returns the object currently being edited by this builder. |
GetTerminator | Gets the terminator of the leader. |
SetBendPoints | Set bending points for polyline to render the leader line. |
SetMinNodeSize | Sets the minimum node size values |
SetOwningSheet | Set the owning sheet when the sheet element is created. |
SetTerminator | Sets the terminator of the leader. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LeaderLineBuilderVerticalAlignmentOption Enumeration | Represents the option NXOpen.Diagramming.LeaderLineBuilder.VerticalAlignment() for a NXOpen.Diagramming.LeaderLineBuilder . |
Property Detail¶
ArrowType¶
-
LeaderLineBuilder.
ArrowType
¶ Returns or sets the arrow type of the end arrow
-------------------------------------
Getter Method
Signature
ArrowType()
Returns: Return type: NXOpen.Diagramming.DiagrammingArrowtype
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowType(arrowTypeOption)
Parameters: arrowTypeOption ( NXOpen.Diagramming.DiagrammingArrowtype
) –New in version NX10.0.0.
License requirements: None.
StubLength¶
-
LeaderLineBuilder.
StubLength
¶ Returns or sets the stub length of this leader line.
The negative value is not expected.
-------------------------------------
Getter Method
Signature
StubLength()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StubLength(stubLength)
Parameters: stubLength (float) – New in version NX10.0.0.
License requirements: None.
StubSides¶
-
LeaderLineBuilder.
StubSides
¶ Returns or sets the stub sides of this leader line.
-------------------------------------
Getter Method
Signature
StubSides()
Returns: Return type: NXOpen.Diagramming.DiagrammingStubsides
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StubSides(stubSides)
Parameters: stubSides ( NXOpen.Diagramming.DiagrammingStubsides
) –New in version NX10.0.0.
License requirements: None.
VerticalAlignment¶
-
LeaderLineBuilder.
VerticalAlignment
¶ Returns or sets the vertical alignment option.
-------------------------------------
Getter Method
Signature
VerticalAlignment()
Returns: Return type: NXOpen.Diagramming.LeaderLineBuilderVerticalAlignmentOption
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VerticalAlignment(alignmentOption)
Parameters: alignmentOption ( NXOpen.Diagramming.LeaderLineBuilderVerticalAlignmentOption
) –New in version NX10.0.0.
License requirements: None.
Method Detail¶
GetBendPoints¶
-
LeaderLineBuilder.
GetBendPoints
¶ Get bending points for polyline to render the leader line.
Signature
GetBendPoints()
Returns: Return type: list of NXOpen.Point2d
New in version NX10.0.0.
License requirements: None.
GetTerminator¶
-
LeaderLineBuilder.
GetTerminator
¶ Gets the terminator of the leader.
Signature
GetTerminator()
Returns: a tuple Return type: A tuple consisting of (terminator, segmentId, percentX, inputX, percentY, inputY). terminator is a NXOpen.Diagramming.SheetElement
. segmentId is a int. percentX is a float. inputX is a float. percentY is a float. inputY is a float.New in version NX11.0.0.
License requirements: None.
SetBendPoints¶
-
LeaderLineBuilder.
SetBendPoints
¶ Set bending points for polyline to render the leader line.
Signature
SetBendPoints(points)
Parameters: points (list of NXOpen.Point2d
) –New in version NX10.0.0.
License requirements: None.
SetTerminator¶
-
LeaderLineBuilder.
SetTerminator
¶ Sets the terminator of the leader.
Signature
SetTerminator(terminator, segmentId, percentX, inputX, percentY, inputY)
Parameters: - terminator (
NXOpen.Diagramming.SheetElement
) – - segmentId (int) –
- percentX (float) –
- inputX (float) –
- percentY (float) –
- inputY (float) –
New in version NX11.0.0.
License requirements: None.
- terminator (
Validate¶
-
LeaderLineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.