TurningOperationBuilder Class¶
-
class
NXOpen.CAM.
TurningOperationBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a Turning Operation Builder
This is an abstract class and cannot be instantiated.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AdditionalCommands | Returns or sets the Additional Commands |
ChannelName | Returns or sets the channel’s name |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
FeedsBuilder | Returns the feeds and speeds builder |
FlipToolAroundHolder | Returns or sets the Flip Tool Around Holder toggle |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MachineCycleSubroutineName | Returns or sets the machine cycle subroutine name |
MotionOutput | Returns or sets the motion output |
MotionOutputBuilder | Returns the motion output builder |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
ReorientToolHolder | Returns or sets the Reorient Tool Holder toggle |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
RotateTrackingPoint | Returns or sets the Rotate Tracking Point toggle |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolHolderAngle | Returns the Tool Holder Angle |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
TrackingPointStatus | Returns or sets the tracking point status |
UpdateIpw | Returns or sets the update IPW mode |
UseMachineCycle | Returns or sets the Use Machine Cycle toggle |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TurningOperationBuilderMotionOutputOptions Enumeration | The motion output options |
TurningOperationBuilderTrackingPointType Enumeration | available types for tracking point |
Property Detail¶
AdditionalCommands¶
-
TurningOperationBuilder.
AdditionalCommands
¶ Returns or sets the Additional Commands
-------------------------------------
Getter Method
Signature
AdditionalCommands()
Returns: the additional commands Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdditionalCommands(additionalCommands)
Parameters: additionalCommands (str) – the additional commands New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
FeedsBuilder¶
-
TurningOperationBuilder.
FeedsBuilder
¶ Returns the feeds and speeds builder
-------------------------------------
Getter Method
Signature
FeedsBuilder()
Returns: the feeds and speeds builder Return type: NXOpen.CAM.FeedsTurnBuilder
New in version NX6.0.0.
License requirements: None.
FlipToolAroundHolder¶
-
TurningOperationBuilder.
FlipToolAroundHolder
¶ Returns or sets the Flip Tool Around Holder toggle
-------------------------------------
Getter Method
Signature
FlipToolAroundHolder()
Returns: the machine’s A-axis Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlipToolAroundHolder(machAAxis)
Parameters: machAAxis (bool) – the machine’s A-axis New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
MachineCycleSubroutineName¶
-
TurningOperationBuilder.
MachineCycleSubroutineName
¶ Returns or sets the machine cycle subroutine name
-------------------------------------
Getter Method
Signature
MachineCycleSubroutineName()
Returns: the machine cycle subroutine name Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MachineCycleSubroutineName(machineCycleSubroutineName)
Parameters: machineCycleSubroutineName (str) – the machine cycle subroutine name New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
MotionOutput¶
-
TurningOperationBuilder.
MotionOutput
¶ Returns or sets the motion output
-------------------------------------
Getter Method
Signature
MotionOutput()
Returns: the motion output Return type: NXOpen.CAM.TurningOperationBuilderMotionOutputOptions
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MotionOutput(motionOutput)
Parameters: motionOutput ( NXOpen.CAM.TurningOperationBuilderMotionOutputOptions
) – the motion outputNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ReorientToolHolder¶
-
TurningOperationBuilder.
ReorientToolHolder
¶ Returns or sets the Reorient Tool Holder toggle
-------------------------------------
Getter Method
Signature
ReorientToolHolder()
Returns: Reorient Tool Holder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReorientToolHolder(reorient)
Parameters: reorient (bool) – Reorient Tool Holder New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RotateTrackingPoint¶
-
TurningOperationBuilder.
RotateTrackingPoint
¶ Returns or sets the Rotate Tracking Point toggle
-------------------------------------
Getter Method
Signature
RotateTrackingPoint()
Returns: Rotate Tracking Point Return type: bool New in version NX7.5.0.
Deprecated since version NX8.5.0: Use
CAM.TurningOperationBuilder.TrackingPointStatus`()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTrackingPoint(rotate)
Parameters: rotate (bool) – Rotate Tracking Point New in version NX7.5.0.
Deprecated since version NX8.5.0: Use
CAM.TurningOperationBuilder.TrackingPointStatus`()
instead.License requirements: cam_base (“CAM BASE”)
ToolHolderAngle¶
-
TurningOperationBuilder.
ToolHolderAngle
¶ Returns the Tool Holder Angle
-------------------------------------
Getter Method
Signature
ToolHolderAngle()
Returns: the Tool Holder Angle builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
TrackingPointStatus¶
-
TurningOperationBuilder.
TrackingPointStatus
¶ Returns or sets the tracking point status
-------------------------------------
Getter Method
Signature
TrackingPointStatus()
Returns: tracking point status Return type: NXOpen.CAM.TurningOperationBuilderTrackingPointType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrackingPointStatus(status)
Parameters: status ( NXOpen.CAM.TurningOperationBuilderTrackingPointType
) – tracking point statusNew in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
UpdateIpw¶
-
TurningOperationBuilder.
UpdateIpw
¶ Returns or sets the update IPW mode
-------------------------------------
Getter Method
Signature
UpdateIpw()
Returns: the update IPW mode Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpdateIpw(updateIpwMode)
Parameters: updateIpwMode (bool) – the update IPW mode New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
UseMachineCycle¶
-
TurningOperationBuilder.
UseMachineCycle
¶ Returns or sets the Use Machine Cycle toggle
-------------------------------------
Getter Method
Signature
UseMachineCycle()
Returns: the machine cycle Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseMachineCycle(machineCycle)
Parameters: machineCycle (bool) – the machine cycle New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
TurningOperationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.