TurningOperationBuilderMotionOutputOptions Enumeration

NXOpen.CAM.TurningOperationBuilder.MotionOutputOptions is an alias for NXOpen.CAM.TurningOperationBuilderMotionOutputOptions

class NXOpen.CAM.TurningOperationBuilderMotionOutputOptions

Bases: object

The motion output options

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
LinearOnly
Linear output only
Circular
Linear and circular motions output
MachineCycle
Machine cycle motions output
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.