TurnThreadEngageRetractBuilder Class

class NXOpen.CAM.TurnThreadEngageRetractBuilder

Bases: NXOpen.TaggedObject

Represents a Thread Turning Engage or Retract Builder

New in version NX6.0.0.

Properties

Property Description
Angle Returns or sets the angle
EngageRetractType Returns or sets the the Engage(Retract) Type
MoveType Returns or sets the Move Type
Tag Returns the Tag for this object.
VectorXc Returns or sets the vector Xc
VectorYc Returns or sets the vector Yc

Methods

Property Detail

Angle

TurnThreadEngageRetractBuilder.Angle

Returns or sets the angle

-------------------------------------

Getter Method

Signature Angle()

Returns:the angle
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Angle(angle)

Parameters:angle (float) – the angle

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

EngageRetractType

TurnThreadEngageRetractBuilder.EngageRetractType

Returns or sets the the Engage(Retract) Type

-------------------------------------

Getter Method

Signature EngageRetractType()

Returns:the the Engage(Retract) Type
Return type:NXOpen.CAM.TurnThreadEngageRetractBuilderEngageRetractTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature EngageRetractType(engageRetractType)

Parameters:engageRetractType (NXOpen.CAM.TurnThreadEngageRetractBuilderEngageRetractTypes) – the the Engage(Retract) Type

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

MoveType

TurnThreadEngageRetractBuilder.MoveType

Returns or sets the Move Type

-------------------------------------

Getter Method

Signature MoveType()

Returns:the Move Type
Return type:NXOpen.CAM.TurnThreadEngageRetractBuilderMoveTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MoveType(moveType)

Parameters:moveType (NXOpen.CAM.TurnThreadEngageRetractBuilderMoveTypes) – the Move Type

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

VectorXc

TurnThreadEngageRetractBuilder.VectorXc

Returns or sets the vector Xc

-------------------------------------

Getter Method

Signature VectorXc()

Returns:the vector Xc
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature VectorXc(vectorXc)

Parameters:vectorXc (float) – the vector Xc

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

VectorYc

TurnThreadEngageRetractBuilder.VectorYc

Returns or sets the vector Yc

-------------------------------------

Getter Method

Signature VectorYc()

Returns:the vector Yc
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature VectorYc(vectorYc)

Parameters:vectorYc (float) – the vector Yc

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)