TurnThreadEngageRetractBuilderMoveTypes Enumeration

NXOpen.CAM.TurnThreadEngageRetractBuilder.MoveTypes is an alias for NXOpen.CAM.TurnThreadEngageRetractBuilderMoveTypes

class NXOpen.CAM.TurnThreadEngageRetractBuilderMoveTypes

Bases: object

The move type

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
Engage
Engage(Retract)
Thread
Thread
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.