TurnThreadEngageRetractBuilderEngageRetractTypes Enumeration

NXOpen.CAM.TurnThreadEngageRetractBuilder.EngageRetractTypes is an alias for NXOpen.CAM.TurnThreadEngageRetractBuilderEngageRetractTypes

class NXOpen.CAM.TurnThreadEngageRetractBuilderEngageRetractTypes

Bases: object

The engage retract type

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
Automatic
Automatic
Vector
Vector
Angle
Angle
SameAsEngage
Same as Engage
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.