TurnRoughFinishLocalReturnBuilder Class

class NXOpen.CAM.TurnRoughFinishLocalReturnBuilder

Bases: NXOpen.TaggedObject

Represents an avoidance start Builder

New in version NX6.0.0.

Properties

Property Description
AdjustmentMode Returns or sets the adjustment mode mode
Distance Returns or sets the local distance value
Dwell Returns or sets the Dwell Time or Revolutions
DwellUnit Returns or sets the Dwell Unit type
EndOfPathBuilder Returns the end event builder
LowerLimit Returns or sets the lower limit
Mode Returns or sets the local return type
NumberOfCuts Returns or sets the local number of cuts
NumberOfLevels Returns or sets the local number of levels
NumberOfPasses Returns or sets the local number of passes value
OperatorMessage Returns or sets the Operator Message String
OutputOperatorMessage Returns or sets the output operator message option
OutputOpskip Returns or sets the output opskip option
OutputOpstop Returns or sets the output opstop option
OutputStop Returns or sets the output stop option
Point Returns or sets the local return point
ReturnMoveMode Returns or sets the adjustment mode mode
StartOfPathBuilder Returns the start event builder
Tag Returns the Tag for this object.
Time Returns or sets the local time value
UpperLimit Returns or sets the upper limit

Methods

Method Description
GetLowerLimitType Get the lower limits mode @return the lower limits mode value
GetUpperLimitType Get the upper limits mode @return the upper limits mode value
SetLowerLimitType Set the lower limits mode
SetUpperLimitType Set the upper limits mode

Property Detail

AdjustmentMode

TurnRoughFinishLocalReturnBuilder.AdjustmentMode

Returns or sets the adjustment mode mode

-------------------------------------

Getter Method

Signature AdjustmentMode()

Returns:the adjustment mode value
Return type:NXOpen.CAM.TurnRoughFinishLocalReturnBuilderAdjustmentModeTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AdjustmentMode(adjustmentMode)

Parameters:adjustmentMode (NXOpen.CAM.TurnRoughFinishLocalReturnBuilderAdjustmentModeTypes) – the adjustment mode value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Distance

TurnRoughFinishLocalReturnBuilder.Distance

Returns or sets the local distance value

-------------------------------------

Getter Method

Signature Distance()

Returns:the local distance value
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Distance(localDistanceValue)

Parameters:localDistanceValue (float) – the local distance value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Dwell

TurnRoughFinishLocalReturnBuilder.Dwell

Returns or sets the Dwell Time or Revolutions

-------------------------------------

Getter Method

Signature Dwell()

Returns:the Dwell Time or Revolutions value
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Dwell(dwell)

Parameters:dwell (float) – the Dwell Time or Revolutions value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

DwellUnit

TurnRoughFinishLocalReturnBuilder.DwellUnit

Returns or sets the Dwell Unit type

-------------------------------------

Getter Method

Signature DwellUnit()

Returns:the Dwell Unit value
Return type:NXOpen.CAM.TurnRoughFinishLocalReturnBuilderDwellUnitTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DwellUnit(dwellUnit)

Parameters:dwellUnit (NXOpen.CAM.TurnRoughFinishLocalReturnBuilderDwellUnitTypes) – the Dwell Unit value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

EndOfPathBuilder

TurnRoughFinishLocalReturnBuilder.EndOfPathBuilder

Returns the end event builder

-------------------------------------

Getter Method

Signature EndOfPathBuilder()

Returns:the end of path builder
Return type:NXOpen.CAM.PostEventsCiBuilder

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

LowerLimit

TurnRoughFinishLocalReturnBuilder.LowerLimit

Returns or sets the lower limit

-------------------------------------

Getter Method

Signature LowerLimit()

Returns:the lower limit value
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LowerLimit(lowerLimitValue)

Parameters:lowerLimitValue (float) – the lower limit value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Mode

TurnRoughFinishLocalReturnBuilder.Mode

Returns or sets the local return type

-------------------------------------

Getter Method

Signature Mode()

Returns:the start local return type value
Return type:NXOpen.CAM.TurnRoughFinishLocalReturnBuilderModeTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Mode(localReturnModeType)

Parameters:localReturnModeType (NXOpen.CAM.TurnRoughFinishLocalReturnBuilderModeTypes) – the start local return type value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

NumberOfCuts

TurnRoughFinishLocalReturnBuilder.NumberOfCuts

Returns or sets the local number of cuts

-------------------------------------

Getter Method

Signature NumberOfCuts()

Returns:the local number of cuts value
Return type:int

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature NumberOfCuts(localNumberOfCutsValue)

Parameters:localNumberOfCutsValue (int) – the local number of cuts value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

NumberOfLevels

TurnRoughFinishLocalReturnBuilder.NumberOfLevels

Returns or sets the local number of levels

-------------------------------------

Getter Method

Signature NumberOfLevels()

Returns:the local number of levels value
Return type:int

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature NumberOfLevels(localNumberOfLevelsValue)

Parameters:localNumberOfLevelsValue (int) – the local number of levels value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

NumberOfPasses

TurnRoughFinishLocalReturnBuilder.NumberOfPasses

Returns or sets the local number of passes value

-------------------------------------

Getter Method

Signature NumberOfPasses()

Returns:the local number of passes value
Return type:int

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature NumberOfPasses(localNumberOfPassesValue)

Parameters:localNumberOfPassesValue (int) – the local number of passes value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

OperatorMessage

TurnRoughFinishLocalReturnBuilder.OperatorMessage

Returns or sets the Operator Message String

-------------------------------------

Getter Method

Signature OperatorMessage()

Returns:the Operator Message String value
Return type:str

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OperatorMessage(operatorMessage)

Parameters:operatorMessage (str) – the Operator Message String value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

OutputOperatorMessage

TurnRoughFinishLocalReturnBuilder.OutputOperatorMessage

Returns or sets the output operator message option

-------------------------------------

Getter Method

Signature OutputOperatorMessage()

Returns:the Operator Message value
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OutputOperatorMessage(operatorMessage)

Parameters:operatorMessage (bool) – the Operator Message value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

OutputOpskip

TurnRoughFinishLocalReturnBuilder.OutputOpskip

Returns or sets the output opskip option

-------------------------------------

Getter Method

Signature OutputOpskip()

Returns:the Opskip value
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OutputOpskip(opskipValue)

Parameters:opskipValue (bool) – the Opskip value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

OutputOpstop

TurnRoughFinishLocalReturnBuilder.OutputOpstop

Returns or sets the output opstop option

-------------------------------------

Getter Method

Signature OutputOpstop()

Returns:the Opstop value
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OutputOpstop(opstopValue)

Parameters:opstopValue (bool) – the Opstop value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

OutputStop

TurnRoughFinishLocalReturnBuilder.OutputStop

Returns or sets the output stop option

-------------------------------------

Getter Method

Signature OutputStop()

Returns:the Stop value
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OutputStop(stopValue)

Parameters:stopValue (bool) – the Stop value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Point

TurnRoughFinishLocalReturnBuilder.Point

Returns or sets the local return point

-------------------------------------

Getter Method

Signature Point()

Returns:the local return point value
Return type:NXOpen.Point

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Point(localReturnPoint)

Parameters:localReturnPoint (NXOpen.Point) – the local return point value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

ReturnMoveMode

TurnRoughFinishLocalReturnBuilder.ReturnMoveMode

Returns or sets the adjustment mode mode

-------------------------------------

Getter Method

Signature ReturnMoveMode()

Returns:the return move mode value
Return type:NXOpen.CAM.TurnRoughFinishLocalReturnBuilderReturnMoveModeTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ReturnMoveMode(returnMoveMode)

Parameters:returnMoveMode (NXOpen.CAM.TurnRoughFinishLocalReturnBuilderReturnMoveModeTypes) – the return move mode value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

StartOfPathBuilder

TurnRoughFinishLocalReturnBuilder.StartOfPathBuilder

Returns the start event builder

-------------------------------------

Getter Method

Signature StartOfPathBuilder()

Returns:the start of path builder
Return type:NXOpen.CAM.PostEventsCiBuilder

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Time

TurnRoughFinishLocalReturnBuilder.Time

Returns or sets the local time value

-------------------------------------

Getter Method

Signature Time()

Returns:the local time value
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Time(localTimeValue)

Parameters:localTimeValue (float) – the local time value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

UpperLimit

TurnRoughFinishLocalReturnBuilder.UpperLimit

Returns or sets the upper limit

-------------------------------------

Getter Method

Signature UpperLimit()

Returns:the upper limit value
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature UpperLimit(upperLimitValue)

Parameters:upperLimitValue (float) – the upper limit value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Method Detail

GetLowerLimitType

TurnRoughFinishLocalReturnBuilder.GetLowerLimitType

Get the lower limits mode

Signature GetLowerLimitType()

Returns:the lower limits mode value
Return type:NXOpen.CAM.TurnRoughFinishLocalReturnBuilderLimitTypes

New in version NX6.0.0.

License requirements: None.

GetUpperLimitType

TurnRoughFinishLocalReturnBuilder.GetUpperLimitType

Get the upper limits mode

Signature GetUpperLimitType()

Returns:the upper limits mode value
Return type:NXOpen.CAM.TurnRoughFinishLocalReturnBuilderLimitTypes

New in version NX6.0.0.

License requirements: None.

SetLowerLimitType

TurnRoughFinishLocalReturnBuilder.SetLowerLimitType

Set the lower limits mode

Signature SetLowerLimitType(lowerLimitModeValue)

Parameters:lowerLimitModeValue (NXOpen.CAM.TurnRoughFinishLocalReturnBuilderLimitTypes) – the lower limits mode value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

SetUpperLimitType

TurnRoughFinishLocalReturnBuilder.SetUpperLimitType

Set the upper limits mode

Signature SetUpperLimitType(upperLimitModeValue)

Parameters:upperLimitModeValue (NXOpen.CAM.TurnRoughFinishLocalReturnBuilderLimitTypes) – the upper limits mode value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)