PostEventsCiBuilder Class¶
-
class
NXOpen.CAM.
PostEventsCiBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a PostEventsCiBuilder
New in version NX5.0.1.
Properties¶
Property | Description |
---|---|
PostEvent | Returns or sets the start/end of path toggle |
Tag | Returns the Tag for this object. |
UdeSet | Returns the UdeSet |
Methods¶
Property Detail¶
PostEvent¶
-
PostEventsCiBuilder.
PostEvent
¶ Returns or sets the start/end of path toggle
-------------------------------------
Getter Method
Signature
PostEvent()
Returns: the start/end of path toggle value Return type: bool New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
PostEvent(postTog)
Parameters: postTog (bool) – the start/end of path toggle value New in version NX5.0.1.
License requirements: cam_base (“CAM BASE”)
UdeSet¶
-
PostEventsCiBuilder.
UdeSet
¶ Returns the UdeSet
-------------------------------------
Getter Method
Signature
UdeSet()
Returns: the ude set Return type: NXOpen.CAM.UdeSet
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)