TurnRoughFinishLocalReturnBuilderReturnMoveModeTypes Enumeration¶
NXOpen.CAM.TurnRoughFinishLocalReturnBuilder.ReturnMoveModeTypes is an alias for NXOpen.CAM.TurnRoughFinishLocalReturnBuilderReturnMoveModeTypes
-
class
NXOpen.CAM.
TurnRoughFinishLocalReturnBuilderReturnMoveModeTypes
¶ Bases:
object
the return move mode options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description NotSet Return Move: NoveDirect Return Move: DirectRadialAxial Return Move: Radial-AxialAxialRadial Return Move: Axial-RadialClearRadialDirect Return Move: Clear Radial-DirectClearAxialDirect Return Move: Clear Axial-DirectClearRadial Return Move: Clear RadialClearAxial Return Move: Clear AxialRadialClearAxialDirect Return Move: Radial-Clear Axial-DirectRadialAxialRadial Return Move: Radial-Axial-RadialRadialClearAxial Return Move: Radial-Clear AxialClearRadialClearAxialDirect Return Move: Clear Radial-Clear Axial-DirectClearRadialAxialRadial Return Move: Clear Radial-Axial-RadialClearRadialClearAxial Return Move: Clear Radial-Clear AxialSameAsDeparture Return Move: Same as Departure.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-