TurnOrientWcs Class

class NXOpen.CAM.TurnOrientWcs

Bases: NXOpen.TaggedObject

Represents an Turn Orient Wcs Builder

This is an abstract class, and cannot be instantiated.

New in version NX7.5.0.

Properties

Property Description
Tag Returns the Tag for this object.
WcsOffset Returns or sets the offset of the WCS origin
XcMapping Returns or sets the XC mapping
YcMapping Returns or sets the YC mapping

Methods

Enumerations

TurnOrientWcsXcMappingTypes Enumeration the XC mapping types
TurnOrientWcsYcMappingTypes Enumeration the YC mapping types

Property Detail

WcsOffset

TurnOrientWcs.WcsOffset

Returns or sets the offset of the WCS origin

-------------------------------------

Getter Method

Signature WcsOffset()

Returns:Offset of the WCS origin along the spindle axis
Return type:float

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature WcsOffset(wcsOffset)

Parameters:wcsOffset (float) – Offset of the WCS origin along the spindle axis

New in version NX7.5.0.

License requirements: None.

XcMapping

TurnOrientWcs.XcMapping

Returns or sets the XC mapping

-------------------------------------

Getter Method

Signature XcMapping()

Returns:XC mapping to an MCS axis
Return type:NXOpen.CAM.TurnOrientWcsXcMappingTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature XcMapping(xcMapping)

Parameters:xcMapping (NXOpen.CAM.TurnOrientWcsXcMappingTypes) – XC mapping to an MCS axis

New in version NX7.5.0.

License requirements: None.

YcMapping

TurnOrientWcs.YcMapping

Returns or sets the YC mapping

-------------------------------------

Getter Method

Signature YcMapping()

Returns:YC mapping to an MCS axis
Return type:NXOpen.CAM.TurnOrientWcsYcMappingTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature YcMapping(ycMapping)

Parameters:ycMapping (NXOpen.CAM.TurnOrientWcsYcMappingTypes) – YC mapping to an MCS axis

New in version NX7.5.0.

License requirements: None.