TurnOrientWcsXcMappingTypes Enumeration

NXOpen.CAM.TurnOrientWcs.XcMappingTypes is an alias for NXOpen.CAM.TurnOrientWcsXcMappingTypes

class NXOpen.CAM.TurnOrientWcsXcMappingTypes

Bases: object

the XC mapping types

Enum Members

Enum Member Enum Member Description
SpindleAxis
Map XC to ZM or XM of the MCS
ReversedSpindleAxis
Map XC to -ZM or -XM of the MCS
RadialAxis
Map XC to XM or YM of the MCS
ReversedRadialAxis
Map XC to -XM or -YM of the MCS
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.