TurnOrientWcsYcMappingTypes Enumeration¶
NXOpen.CAM.TurnOrientWcs.YcMappingTypes is an alias for NXOpen.CAM.TurnOrientWcsYcMappingTypes
-
class
NXOpen.CAM.
TurnOrientWcsYcMappingTypes
¶ Bases:
object
the YC mapping types
Enum Members
Enum Member Enum Member Description RadialAxis Map YC to XM or YM of the MCSReversedRadialAxis Map YC to -XM or -YM of the MCSSpindleAxis Map YC to ZM or XM of the MCSReversedSpindleAxis Map YC to -ZM or -XM of the MCS-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-