ToolPathTiltAvoidance Class¶
-
class
NXOpen.CAM.
ToolPathTiltAvoidance
¶ Bases:
NXOpen.Builder
Represents a Tool Path Tilt Avoidance Builder
This is a sub-builder class and cannot be directly instantiated
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AvoidanceMethod | Returns or sets the avoidance method |
FanDistance | Returns the fan distance |
MaintainTilt | Returns or sets the maintain tilt |
MaxMaintainTiltDistance | Returns the max maintain tilt distance |
PreferredTiltAngle | Returns or sets the preferred tilt angle |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ToolPathTiltAvoidanceAxisType Enumeration | the tilting axis type |
ToolPathTiltAvoidanceMethodType Enumeration | the collision avoidance method type |
Property Detail¶
AvoidanceMethod¶
-
ToolPathTiltAvoidance.
AvoidanceMethod
¶ Returns or sets the avoidance method
-------------------------------------
Getter Method
Signature
AvoidanceMethod()
Returns: the avoidance method type Return type: NXOpen.CAM.ToolPathTiltAvoidanceMethodType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AvoidanceMethod(referenceType)
Parameters: referenceType ( NXOpen.CAM.ToolPathTiltAvoidanceMethodType
) – the tilting reference typeNew in version NX9.0.0.
License requirements: None.
FanDistance¶
-
ToolPathTiltAvoidance.
FanDistance
¶ Returns the fan distance
-------------------------------------
Getter Method
Signature
FanDistance()
Returns: the fan distance value Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX9.0.0.
License requirements: None.
MaintainTilt¶
-
ToolPathTiltAvoidance.
MaintainTilt
¶ Returns or sets the maintain tilt
-------------------------------------
Getter Method
Signature
MaintainTilt()
Returns: the value of maintain tilt Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaintainTilt(maintainTilt)
Parameters: maintainTilt (bool) – the value of maintain tilt New in version NX9.0.0.
License requirements: None.
MaxMaintainTiltDistance¶
-
ToolPathTiltAvoidance.
MaxMaintainTiltDistance
¶ Returns the max maintain tilt distance
-------------------------------------
Getter Method
Signature
MaxMaintainTiltDistance()
Returns: the max maintain tilt distance Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX9.0.0.
License requirements: None.
PreferredTiltAngle¶
-
ToolPathTiltAvoidance.
PreferredTiltAngle
¶ Returns or sets the preferred tilt angle
-------------------------------------
Getter Method
Signature
PreferredTiltAngle()
Returns: the value of preferred tilt angle Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PreferredTiltAngle(preferredAngle)
Parameters: preferredAngle (float) – the value of preferred tilt angle New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ToolPathTiltAvoidance.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.