ToolPathTiltAvoidanceMethodType Enumeration

NXOpen.CAM.ToolPathTiltAvoidance.MethodType is an alias for NXOpen.CAM.ToolPathTiltAvoidanceMethodType

class NXOpen.CAM.ToolPathTiltAvoidanceMethodType

Bases: object

the collision avoidance method type

Enum Members

Enum Member Enum Member Description
Tilt
Avoidance method: tilt
Retract
Avoidance method: retract
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.