ToolPathTiltAvoidanceAxisType Enumeration

NXOpen.CAM.ToolPathTiltAvoidance.AxisType is an alias for NXOpen.CAM.ToolPathTiltAvoidanceAxisType

class NXOpen.CAM.ToolPathTiltAvoidanceAxisType

Bases: object

the tilting axis type

Enum Members

Enum Member Enum Member Description
ThreeToFive
the tilting axis reference: three to five
FiveToFive
the tilting axis reference: five to five
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.