PlanarOperationBuilder Class¶
-
class
NXOpen.CAM.
PlanarOperationBuilder
¶ Bases:
NXOpen.CAM.MillOperationBuilder
Represents a PlanarOperation Builder
This is an abstract class and cannot be instantiated.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AdditionalPasses | Returns or sets the Boundary Additional Passes |
AutomaticPartBoundaryMethod | Returns or sets the Automatic Part Boundary Method |
BndStepover | Returns the boundary stepover builder |
ChannelName | Returns or sets the channel’s name |
CheckGeometry | Returns the check geometry builder |
CornerLoops | Returns or sets the corner loops value |
CutAreaGeometry | Returns the cut area geometry builder |
CutParameters | Returns the cut parameter object |
CutPattern | Returns the cut pattern builder |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
DeferCuttingStatus | Returns or sets the defer cutting status value |
DepthPerCut | Returns the depth per cut builder (inheritable double) |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
FeedsBuilder | Returns the feeds and speeds builder |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MinCutLength | Returns the min cut length builder (tool dependent double) |
MotionOutput | Returns the motion output builder |
MotionOutputBuilder | Returns the motion output builder |
NonCuttingBuilder | Returns the non-cutting moves builder |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PartGeometry | Returns the part geometry builder |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
ReferenceTool | Returns or sets the reference tool object |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolAxisFix | Returns the pmop tool axis ci builder |
ToolChangeSetting | Returns the tool change builder |
ToolMinimumLengthUsage | Returns or sets the tool minimum length usage |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PlanarOperationBuilderAutomaticPartBoundaryMethodTypes Enumeration | Available types for automatic part boundary method in planar mill operation |
Property Detail¶
AdditionalPasses¶
-
PlanarOperationBuilder.
AdditionalPasses
¶ Returns or sets the Boundary Additional Passes
-------------------------------------
Getter Method
Signature
AdditionalPasses()
Returns: the Boundary Additional Passes Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdditionalPasses(numPasses)
Parameters: numPasses (int) – the Boundary Additional Passes New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
AutomaticPartBoundaryMethod¶
-
PlanarOperationBuilder.
AutomaticPartBoundaryMethod
¶ Returns or sets the Automatic Part Boundary Method
-------------------------------------
Getter Method
Signature
AutomaticPartBoundaryMethod()
Returns: Return type: NXOpen.CAM.PlanarOperationBuilderAutomaticPartBoundaryMethodTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutomaticPartBoundaryMethod(automaticPartBoundary)
Parameters: automaticPartBoundary ( NXOpen.CAM.PlanarOperationBuilderAutomaticPartBoundaryMethodTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
BndStepover¶
-
PlanarOperationBuilder.
BndStepover
¶ Returns the boundary stepover builder
-------------------------------------
Getter Method
Signature
BndStepover()
Returns: The boundary stepover builder Return type: NXOpen.CAM.StepoverBuilder
New in version NX5.0.0.
License requirements: None.
CheckGeometry¶
-
PlanarOperationBuilder.
CheckGeometry
¶ Returns the check geometry builder
-------------------------------------
Getter Method
Signature
CheckGeometry()
Returns: Return type: NXOpen.CAM.Geometry
New in version NX8.0.0.
License requirements: None.
CornerLoops¶
-
PlanarOperationBuilder.
CornerLoops
¶ Returns or sets the corner loops value
-------------------------------------
Getter Method
Signature
CornerLoops()
Returns: the corner loops value Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerLoops(cornerLoops)
Parameters: cornerLoops (bool) – the corner loops value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CutAreaGeometry¶
-
PlanarOperationBuilder.
CutAreaGeometry
¶ Returns the cut area geometry builder
-------------------------------------
Getter Method
Signature
CutAreaGeometry()
Returns: Return type: NXOpen.CAM.Geometry
New in version NX8.0.0.
License requirements: None.
CutPattern¶
-
PlanarOperationBuilder.
CutPattern
¶ Returns the cut pattern builder
-------------------------------------
Getter Method
Signature
CutPattern()
Returns: The cut pattern builder Return type: NXOpen.CAM.CutPatternBuilder
New in version NX6.0.0.
License requirements: None.
DeferCuttingStatus¶
-
PlanarOperationBuilder.
DeferCuttingStatus
¶ Returns or sets the defer cutting status value
-------------------------------------
Getter Method
Signature
DeferCuttingStatus()
Returns: the defer cutting status value Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeferCuttingStatus(deferCuttingStatus)
Parameters: deferCuttingStatus (bool) – the defer cutting status value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
DepthPerCut¶
-
PlanarOperationBuilder.
DepthPerCut
¶ Returns the depth per cut builder (inheritable double)
-------------------------------------
Getter Method
Signature
DepthPerCut()
Returns: the depth per cut builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: None.
NonCuttingBuilder¶
-
PlanarOperationBuilder.
NonCuttingBuilder
¶ Returns the non-cutting moves builder
-------------------------------------
Getter Method
Signature
NonCuttingBuilder()
Returns: Return type: NXOpen.CAM.NcmPlanarBuilder
New in version NX5.0.0.
License requirements: None.
PartGeometry¶
-
PlanarOperationBuilder.
PartGeometry
¶ Returns the part geometry builder
-------------------------------------
Getter Method
Signature
PartGeometry()
Returns: Return type: NXOpen.CAM.Geometry
New in version NX8.0.0.
License requirements: None.
ToolAxisFix¶
-
PlanarOperationBuilder.
ToolAxisFix
¶ Returns the pmop tool axis ci builder
-------------------------------------
Getter Method
Signature
ToolAxisFix()
Returns: Return type: NXOpen.CAM.ToolAxisFixed
New in version NX7.5.0.
License requirements: None.
ToolMinimumLengthUsage¶
-
PlanarOperationBuilder.
ToolMinimumLengthUsage
¶ Returns or sets the tool minimum length usage
-------------------------------------
Getter Method
Signature
ToolMinimumLengthUsage()
Returns: the tool minimum length usage Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolMinimumLengthUsage(toolMinUsage)
Parameters: toolMinUsage (bool) – the tool minimum length usage New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
PlanarOperationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.