PlanarOperationBuilderAutomaticPartBoundaryMethodTypes Enumeration

NXOpen.CAM.PlanarOperationBuilder.AutomaticPartBoundaryMethodTypes is an alias for NXOpen.CAM.PlanarOperationBuilderAutomaticPartBoundaryMethodTypes

class NXOpen.CAM.PlanarOperationBuilderAutomaticPartBoundaryMethodTypes

Bases: object

Available types for automatic part boundary method in planar mill operation

Enum Members

Enum Member Enum Member Description
FollowWallBottom
Follow Bottom
FollowWallTop
Follow Top
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.