NcmTurnRoughFinishBuilder Class¶
-
class
NXOpen.CAM.
NcmTurnRoughFinishBuilder
¶ Bases:
NXOpen.CAM.NcmTurningBuilder
Represents a CAM.
NcmTurnRoughFinishBuilder .. versionadded:: NX6.0.0
Properties¶
Property | Description |
---|---|
AvoidanceAfterLastRetract | Returns or sets the prefer direct motion after last retract |
AvoidanceApproachBuilder | Returns the approach path builder |
AvoidanceBetweenRegions | Returns or sets the prefer direct motion between regions |
AvoidanceClearanceBuilder | Returns the clearance builder |
AvoidanceDepartureBuilder | Returns the departure path builder |
AvoidanceForAutomaticEngage | Returns or sets the additional checking for automatic engage |
AvoidanceForAutomaticRetract | Returns or sets the additional checking for automatic retract |
AvoidanceForMinimumClearance | Returns or sets the additional checking for minimum clearance |
AvoidanceFromBuilder | Returns the avoidance from builder |
AvoidanceGohomeBuilder | Returns the gohome point builder |
AvoidanceReturnBuilder | Returns the return path builder |
AvoidanceStartBuilder | Returns the avoidance start builder |
AvoidanceStartOfEngageBuilder | Returns the start of engage builder |
AvoidanceToStartOfEngage | Returns or sets the prefer direct motion to start of engage |
AxialSafeClearance | Returns or sets the axial safe clearance value |
Cutcom | Returns the cutter compensation builder |
DefaultRegionStartType | Returns or sets the region start type |
EngageProfileBuilder | Returns the Profiling Engage builder |
LocalReturnBuilder | Returns the Local Return builder |
NcmHoleMachiningBuilder | Returns the non cutting moves hole machining builder |
RadialSafeClearance | Returns or sets the radial safe clearance value |
RetractProfileBuilder | Returns the Profiling Retract builder |
StartPointsEffectDistBuilder | Returns the region start points effective distance builder (inheritable tool dep) |
StartPointsUseEffectDist | Returns or sets the start points use effective distance |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetRegionStartPoints | Returns region start points |
SetRegionStartPoints | Sets region start points |
Property Detail¶
AvoidanceForAutomaticEngage¶
-
NcmTurnRoughFinishBuilder.
AvoidanceForAutomaticEngage
¶ Returns or sets the additional checking for automatic engage
-------------------------------------
Getter Method
Signature
AvoidanceForAutomaticEngage()
Returns: the additional checking for automatic engage Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AvoidanceForAutomaticEngage(avoidanceAutomaticEngage)
Parameters: avoidanceAutomaticEngage (bool) – the additional checking for automatic engage New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceForAutomaticRetract¶
-
NcmTurnRoughFinishBuilder.
AvoidanceForAutomaticRetract
¶ Returns or sets the additional checking for automatic retract
-------------------------------------
Getter Method
Signature
AvoidanceForAutomaticRetract()
Returns: the additional checking for automatic retract Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AvoidanceForAutomaticRetract(avoidanceAutomaticRetract)
Parameters: avoidanceAutomaticRetract (bool) – the additional checking for automatic retract New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceForMinimumClearance¶
-
NcmTurnRoughFinishBuilder.
AvoidanceForMinimumClearance
¶ Returns or sets the additional checking for minimum clearance
-------------------------------------
Getter Method
Signature
AvoidanceForMinimumClearance()
Returns: the additional checking for minimum clearance Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AvoidanceForMinimumClearance(avoidanceMinimumClearance)
Parameters: avoidanceMinimumClearance (bool) – the additional checking for minimum clearance New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AxialSafeClearance¶
-
NcmTurnRoughFinishBuilder.
AxialSafeClearance
¶ Returns or sets the axial safe clearance value
-------------------------------------
Getter Method
Signature
AxialSafeClearance()
Returns: the axial safe clearance value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxialSafeClearance(axialSafeClearanceValue)
Parameters: axialSafeClearanceValue (float) – the axial safe clearance value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
EngageProfileBuilder¶
-
NcmTurnRoughFinishBuilder.
EngageProfileBuilder
¶ Returns the Profiling Engage builder
-------------------------------------
Getter Method
Signature
EngageProfileBuilder()
Returns: the Profiling Engage builder Return type: NXOpen.CAM.TurnEngageRetractBuilder
New in version NX6.0.0.
License requirements: None.
LocalReturnBuilder¶
-
NcmTurnRoughFinishBuilder.
LocalReturnBuilder
¶ Returns the Local Return builder
-------------------------------------
Getter Method
Signature
LocalReturnBuilder()
Returns: the Local Return builder Return type: NXOpen.CAM.TurnRoughFinishLocalReturnBuilder
New in version NX6.0.0.
License requirements: None.
RadialSafeClearance¶
-
NcmTurnRoughFinishBuilder.
RadialSafeClearance
¶ Returns or sets the radial safe clearance value
-------------------------------------
Getter Method
Signature
RadialSafeClearance()
Returns: the radial safe clearance value Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialSafeClearance(radialSafeClearanceValue)
Parameters: radialSafeClearanceValue (float) – the radial safe clearance value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RetractProfileBuilder¶
-
NcmTurnRoughFinishBuilder.
RetractProfileBuilder
¶ Returns the Profiling Retract builder
-------------------------------------
Getter Method
Signature
RetractProfileBuilder()
Returns: the Profiling Retract builder Return type: NXOpen.CAM.TurnEngageRetractBuilder
New in version NX6.0.0.
License requirements: None.