NcmSubopBuilder Class¶
-
class
NXOpen.CAM.
NcmSubopBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.NcmSubopBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DefaultRegionStartType | Returns or sets the region start type |
StartPointsEffectDistBuilder | Returns the region start points effective distance builder (inheritable tool dep) |
StartPointsUseEffectDist | Returns or sets the start points use effective distance |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetRegionStartPoints | Returns region start points |
SetRegionStartPoints | Sets region start points |
Enumerations¶
NcmSubopBuilderDefaultRegionStartTypes Enumeration | Available types for default region start in subop milling |
Property Detail¶
DefaultRegionStartType¶
-
NcmSubopBuilder.
DefaultRegionStartType
¶ Returns or sets the region start type
-------------------------------------
Getter Method
Signature
DefaultRegionStartType()
Returns: Return type: NXOpen.CAM.NcmSubopBuilderDefaultRegionStartTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultRegionStartType(defaultRegionStartType)
Parameters: defaultRegionStartType ( NXOpen.CAM.NcmSubopBuilderDefaultRegionStartTypes
) –New in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
StartPointsEffectDistBuilder¶
-
NcmSubopBuilder.
StartPointsEffectDistBuilder
¶ Returns the region start points effective distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
StartPointsEffectDistBuilder()
Returns: The start points effective distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX8.5.0.
License requirements: None.
StartPointsUseEffectDist¶
-
NcmSubopBuilder.
StartPointsUseEffectDist
¶ Returns or sets the start points use effective distance
-------------------------------------
Getter Method
Signature
StartPointsUseEffectDist()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPointsUseEffectDist(newValue)
Parameters: newValue (bool) – New in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetRegionStartPoints¶
-
NcmSubopBuilder.
GetRegionStartPoints
¶ Returns region start points
Signature
GetRegionStartPoints()
Returns: The points Return type: list of NXOpen.Point
New in version NX8.5.0.
License requirements: None.
SetRegionStartPoints¶
-
NcmSubopBuilder.
SetRegionStartPoints
¶ Sets region start points
Signature
SetRegionStartPoints(regionStartPoints)
Parameters: regionStartPoints (list of NXOpen.Point
) – The pointsNew in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)