IpwAnalysisBuilder Class

class NXOpen.CAM.IpwAnalysisBuilder

Bases: NXOpen.Builder

Represents a NXOpen.CAM.IpwAnalysisBuilder

This is an abstract class, and cannot be instantiated.

New in version NX6.0.0.

Properties

Property Description
ColorControlType Returns or sets the control color
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
CreateIpwContainmentCurvesBuilder Creates a list item @return ipw containment curves builder
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

IpwAnalysisBuilderColorControl Enumeration the color control type options

Property Detail

ColorControlType

IpwAnalysisBuilder.ColorControlType

Returns or sets the control color

-------------------------------------

Getter Method

Signature ColorControlType()

Returns:
Return type:NXOpen.CAM.IpwAnalysisBuilderColorControl

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ColorControlType(type)

Parameters:type (NXOpen.CAM.IpwAnalysisBuilderColorControl) –

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Method Detail

CreateIpwContainmentCurvesBuilder

IpwAnalysisBuilder.CreateIpwContainmentCurvesBuilder

Creates a list item

Signature CreateIpwContainmentCurvesBuilder(position)

Parameters:position (int) – position
Returns:ipw containment curves builder
Return type:NXOpen.CAM.IpwContainmentCurvesBuilder

New in version NX6.0.0.

License requirements: None.

Validate

IpwAnalysisBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.