IpwAnalysisBuilderColorControl Enumeration

NXOpen.CAM.IpwAnalysisBuilder.ColorControl is an alias for NXOpen.CAM.IpwAnalysisBuilderColorControl

class NXOpen.CAM.IpwAnalysisBuilderColorControl

Bases: object

the color control type options

Enum Members

Enum Member Enum Member Description
Sharp
use blend color control
Blend
use sharp color control
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.