IpwContainmentCurvesBuilder Class¶
-
class
NXOpen.CAM.
IpwContainmentCurvesBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAM.IpwContainmentCurvesBuilder
This is an abstract class, and cannot be instantiated.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
FeatureName | Returns or sets the feature name |
SmoothingTolerance | Returns or sets the smoothing tolerance |
SpecifyDistance | Returns or sets the specify distance |
SpecifyPoint | Returns or sets the specify point |
Tag | Returns the Tag for this object. |
ThicknessMode | Returns or sets the thickness mode |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
IpwContainmentCurvesBuilderThicknessModeValue Enumeration | the thickness method options |
Property Detail¶
FeatureName¶
-
IpwContainmentCurvesBuilder.
FeatureName
¶ Returns or sets the feature name
-------------------------------------
Getter Method
Signature
FeatureName()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureName(featureName)
Parameters: featureName (str) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
SmoothingTolerance¶
-
IpwContainmentCurvesBuilder.
SmoothingTolerance
¶ Returns or sets the smoothing tolerance
-------------------------------------
Getter Method
Signature
SmoothingTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothingTolerance(smoothingTolerance)
Parameters: smoothingTolerance (float) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
SpecifyDistance¶
-
IpwContainmentCurvesBuilder.
SpecifyDistance
¶ Returns or sets the specify distance
-------------------------------------
Getter Method
Signature
SpecifyDistance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecifyDistance(distanceValue)
Parameters: distanceValue (float) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
SpecifyPoint¶
-
IpwContainmentCurvesBuilder.
SpecifyPoint
¶ Returns or sets the specify point
-------------------------------------
Getter Method
Signature
SpecifyPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecifyPoint(point)
Parameters: point ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ThicknessMode¶
-
IpwContainmentCurvesBuilder.
ThicknessMode
¶ Returns or sets the thickness mode
-------------------------------------
Getter Method
Signature
ThicknessMode()
Returns: Return type: NXOpen.CAM.IpwContainmentCurvesBuilderThicknessModeValue
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessMode(method)
Parameters: method ( NXOpen.CAM.IpwContainmentCurvesBuilderThicknessModeValue
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
IpwContainmentCurvesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.