IpwContainmentCurvesBuilderThicknessModeValue Enumeration

NXOpen.CAM.IpwContainmentCurvesBuilder.ThicknessModeValue is an alias for NXOpen.CAM.IpwContainmentCurvesBuilderThicknessModeValue

class NXOpen.CAM.IpwContainmentCurvesBuilderThicknessModeValue

Bases: object

the thickness method options

Enum Members

Enum Member Enum Member Description
Point
use thickness mode point
Distance
use thickness mode distance
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.